DOCA0384EN-01

Configuration of the M2C/M6C Programmable Contacts

General Description

The M2C and M6C programmable contacts may be used to signal pick-up value overruns or status changes:

  • M2C has two contacts, 1 and 2

  • M6C has six contacts, 1 to 6

The M2C/M6C programmable contacts can be configured:

  • locally via the HMI of the MicroLogic P/H trip unit

  • remotely via the communication interface

The remote configuration of each contact can be allowed or forbidden by the local configuration via the HMI of the MicroLogic P/H trip unit with a firmware version > 2009 AJ.

Remote Configuration Status

Address

Register

RW

X

Unit

Type

Range

A/E/P/H

Description

0x2647

9800

R

INT16U

0–1

P/H

Remote configuration status:

0 = indicates that remote configuration of the contact is not authorized (factory setting).

1 = indicates that remote configuration of the contact is authorized.

Remote configuration status can be modified only locally via the HMI of MicroLogic P/H trip unit.

M2C/M6C Programmable Contact Registers

The settings of the M2C/M6C programmable contacts are in the contact registers:

Contact Number

Contact Addresses

Contact Registers

1

0x2648–0x264E

9801–9807

2

0x264F–0x2655

9808–9814

3

0x2656–0x265C

9815–9821

4

0x265D–0x2663

9822–9828

5

0x2664–0x266A

9829–9835

6

0x266B–0x2671

9836–9842

M2C/M6C Programmable Contact 1 Description

The order and the description of the M2C/M6C programmable contacts are the same as that of contact 1:

Address

Register

RW

X

Unit

Type

Range

A/E/P/H

Description

0x2648

9801

RW

INT16U

0–4

Output mode

E/P/H

0 = normal (non-latching) mode (factory setting)

Contact closed each time for as long as the assigned alarm remains active.

P/H

1 = latching mode

Contact closed for each assigned alarm and remains activated until the alarm is reset by the user (through the command interface or by a reset on the trip unit).

P/H

2 = time delay mode

Contact closed for a set time for each assigned alarm. It is opened at the end of the time delay whether the alarm is still active or not. The alarm must change status at least once to open the contact again.

E/P/H

3 = forced to 1

The contact remains closed and is not controlled by the alarm status.

E/P/H

4 = forced to 0

The contact remains open and is not controlled by the alarm status.

0x2649

9802

RW

10

s

INT16U

10– 3600

P/H

Contact activation time delay for time-delay mode

Factory setting: 3600 (360 s)

0x264A–0x264D

9803– 9806

RW

OCTET STRING

0x00– 0x7F

P/H

Contact name in ASCII (A–Z and 0–9) using 4 registers

Update via the trip unit not possible

Factory setting: ‘set up !’

0x264E

9807

RW

INT16U

1000– 1031

E/P/H

Owner alarm number for the contact 1.

Factory setting = 0x8000 (no owner)

Type of Programmable Contacts

Address

Register

RW

X

Unit

Type

Range

A/E/P/H

Description

0x2672

9843

R

INT16U

0–6

E/P/H

0 = none

E/P/H

2 = M2C

P/H

6 = M6C

Event Assignment to M2C/M6C Programmable Contacts

The M2C/M6C programmable contacts can be associated to a basic or advanced protection parameter event.

Depending on the protection parameter, a specific register can contain the programmable contact number which opens or closes at the end of the protection time delay (register 8763 as example).

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?