DOCA0384EN-01

Energy Measurements

General Description

Energy measurements include:

  • active energy Ep

  • reactive energy Eq

  • apparent energy Es

  • active energy counted positively (EpIn) or negatively (EpOut), according to the configuration of register 3316 Power Flow Sign

  • reactive energy counted positively (EqIn) or negatively (EqOut), according to the configuration of register 3316 Power Flow Sign

  • active energy and reactive energy are accumulated according to the configuration of register 3324 (absolute mode by factory setting) Energy Accumulation Mode

The reset minimum/maximum command (command code = 46728) can reset the content of the energy measurement registers.

Address

Register

RW

X

Unit

Type

Range

A/E/P/H

Description

0x07CF–0x07D2

2000–2003

R

1

kWh

MOD 10000

-1016 to +1016

E/P/H

Total active energy: Ep (1)

0x07D3–0x07D6

2004–2007

R

1

kVARh

MOD 10000

-1016 to +1016

E/P/H

Total reactive energy: Eq (1)

0x07D7–0x07DA

2008–2011

R

1

kWh

MOD 10000

-1016 to +1016

P/H

Active energy counted positively: EpIn

0x07DB–0x07DE

2012–2015

R

1

kWh

MOD 10000

-1016 to +1016

P/H

Active energy counted negatively: EpOut

0x07DF–0x07E2

2016–2019

R

1

kVARh

MOD 10000

-1016 to +1016

P/H

Reactive energy counted positively: EqIn

0x07E3–0x07E6

2020–2023

R

1

kVARh

MOD 10000

-1016 to +1016

P/H

Reactive energy counted negatively: EqOut

0x07E7–0x07EA

2024–2027

R

1

kVAh

MOD 10000

-1016 to +1016

E/P/H

Total apparent energy: Es

(1) Total active energy and total reactive energy are always counted positively with MicroLogic E trip unit.

NOTE:
  • The MicroLogic E trip unit screen displays positive values (only) up to 999 999 999 kWh. Over this value, MicroLogic E trip unit screen displays 999 999 999 kWh.

  • The MicroLogic P or H trip unit screen displays positive values up to 99 999 999 kWh. Over this value, MicroLogic P or H trip unit screen displays 0 and then 1 kWh.

  • The MicroLogic P or H trip unit screen displays negative values up to -99 999 999 kWh. Over this value, MicroLogic P or H trip unit screen displays 0 and then -1 kWh.

  • MOD10000 format is explained in the data type description.

The behavior is the same for reactive energy and apparent energy.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?