Analog Predefined Alarms
General Description
The EcoStruxure Power Commission software enables the configuration of analog predefined alarms.
Analog predefined alarms:
-
may be modified via the command interface in configuration mode
-
are only available with a MicroLogic H trip unit
-
can be used to trigger waveform capture
Analog Predefined Alarms Number
The following table describes the list of predefined alarms and corresponding numbers, registers, and addresses.
|
Alarm Number |
Alarm Addresses |
Alarm Registers |
Alarm Description |
|---|---|---|---|
|
1 |
0x176F–0x177A |
6000–6011 |
Overcurrent phase 1 |
|
2 |
0x177B–0x1786 |
6012–6023 |
Overcurrent phase 2 |
|
3 |
0x1787–0x1792 |
6024–6035 |
Overcurrent phase 3 |
|
4 |
0x1793–0x179E |
6036–6047 |
Over neutral current |
|
5 |
0x179F–0x17AA |
6048–6059 |
Over ground current |
|
6 |
0x17AB–0x17B6 |
6060–6071 |
Undercurrent phase 1 |
|
7 |
0x17B7–0x17C2 |
6072–6083 |
Undercurrent phase 2 |
|
8 |
0x17C3–0x17CE |
6084–6095 |
Undercurrent phase 3 |
|
9 |
0x17CF–0x17DA |
6096–6107 |
Overcurrent unbalance phase 1 |
|
10 |
0x17DB–0x17E6 |
6108–6119 |
Overcurrent unbalance phase 2 |
|
11 |
0x17E7–0x17F2 |
6120–6131 |
Overcurrent unbalance phase 3 |
|
12 |
0x17F3–0x17FE |
6132–6143 |
Overvoltage phase 1 |
|
13 |
0x17FF–0x180A |
6144–6155 |
Overvoltage phase 2 |
|
14 |
0x180B–0x1816 |
6156–6167 |
Overvoltage phase 3 |
|
15 |
0x1817–0x1822 |
6168–6179 |
Undervoltage phase 1 |
|
16 |
0x1823–0x182E |
6180–6191 |
Undervoltage phase 2 |
|
17 |
0x182F–0x183A |
6192–6203 |
Undervoltage phase 3 |
|
18 |
0x183B–0x1846 |
6204–6215 |
Overvoltage unbalance phase 1 |
|
19 |
0x1847–0x1852 |
6216–6227 |
Overvoltage unbalance phase 2 |
|
20 |
0x1853–0x185E |
6228–6239 |
Overvoltage unbalance phase 3 |
|
21 |
0x185F–0x186A |
6240–6251 |
Over total apparent power |
|
22 |
0x186B–0x1876 |
6252–6263 |
Over total active power |
|
23 |
0x1877–0x1882 |
6264–6275 |
Over total active reverse power |
|
24 |
0x1883–0x188E |
6276–6287 |
Over total reactive power |
|
25 |
0x188F–0x189A |
6288–6299 |
Over total reactive reverse power |
|
26 |
0x189B–0x18A6 |
6300–6311 |
Under total apparent power |
|
27 |
0x18A7–0x18B2 |
6312–6323 |
Under total active power |
|
28 |
0x18B3–0x18BE |
6324–6335 |
Under total active reverse power |
|
29 |
0x18BF–0x18CA |
6336–6347 |
Under total reactive power |
|
30 |
0x18CB–0x18D6 |
6348–6359 |
Under total reactive reverse power |
|
31 |
0x18D7–0x18E2 |
6360–6371 |
Lagging true power factor |
|
32 |
0x18E3–0x18EE |
6372–6383 |
Leading true power factor |
|
33 |
0x18EF–0x18FA |
6384–6395 |
Lagging displacement power factor |
|
34 |
0x18FB–0x1906 |
6396–6407 |
Leading displacement power factor |
|
35 |
0x1907–0x1912 |
6408–6419 |
Over total harmonic distortion current phase 1 |
|
36 |
0x1913–0x191E |
6420–6431 |
Over total harmonic distortion current phase 2 |
|
37 |
0x191F–0x192A |
6432–6443 |
Over total harmonic distortion current phase 3 |
|
38 |
0x192B–0x1936 |
6444–6455 |
Over total harmonic distortion voltage (phase 1 to neutral) |
|
39 |
0x1937–0x1942 |
6456–6467 |
Over total harmonic distortion voltage (phase 2 to neutral) |
|
40 |
0x1943–0x194E |
6468–6479 |
Over total harmonic distortion voltage (phase 3 to neutral) |
|
41 |
0x194F–0x195A |
6480–6491 |
Over total harmonic distortion voltage (phase 1 to 2) |
|
42 |
0x195B–0x1966 |
6492–6503 |
Over total harmonic distortion voltage (phase 2 to 3) |
|
43 |
0x1967–0x1972 |
6504–6515 |
Over total harmonic distortion voltage (phase 3 to 1) |
|
44 |
0x1973–0x197E |
6516–6527 |
Over predicted apparent power demand |
|
45 |
0x197F–0x198A |
6528–6539 |
Over predicted total active power demand |
|
46 |
0x198B–0x1996 |
6540–6551 |
Over predicted total active reverse power demand |
|
47 |
0x1997–0x19A2 |
6552–6563 |
Over predicted total reactive power demand |
|
48 |
0x19A3–0x19AE |
6564–6575 |
Over predicted total reactive reverse power demand |
|
49 |
0x19AF–0x19BA |
6576–6587 |
Under predicted apparent power demand |
|
50 |
0x19BB–0x19C6 |
6588–6599 |
Under predicted total active power demand |
|
51 |
0x19C7–0x19D2 |
6600–6611 |
Under predicted total active reverse power demand |
|
52 |
0x19D3–0x19DE |
6612–6623 |
Under predicted total reactive power demand |
|
53 |
0x19DF–0x19EA |
6624–6635 |
Under predicted total reactive reverse power demand |
Analog Predefined Alarm Record
Analog predefined alarms are coded on 12 registers.
The order and the description of the analog predefined alarms are the same as that of analog predefined alarm 1:
|
Analog Predefined Alarm 1 |
||||||||
|---|---|---|---|---|---|---|---|---|
|
Address |
Register |
RW |
X |
Unit |
Type |
Range |
A/E/P/H |
Description |
|
0x176F |
6000 |
RW |
– |
– |
INT16U |
– |
H |
The MSB gives the activity of the alarm: 0 = On 1 = Off The LSB gives the priority of the alarm: 0, 1, 2, or 3. The factory setting value is 0x0101. Register set to 0 will not log event into the event log (file number 10) and Waveform Capture file (file number 5). |
|
0x1770 |
6001 |
R |
– |
– |
INT16U |
1016 |
H |
Register number which content gets in relation to the pick-up value and to the drop-out value. The factory setting is 1016. |
|
0x1771 |
6002 |
R |
– |
– |
INT16U |
– |
H |
Comparison mode: The MSB indicates Pickup mode. The LSB indicates the Dropout mode. MSB and LSB can be set to 1, 2 or 4:
|
|
0x1772 |
6003 |
RW |
1 |
– |
INT16U |
– |
H |
Alarm actuation pick-up value (1) The factory setting is 0x8000. |
|
0x1773 |
6004 |
R |
100 |
% |
INT16U |
– |
H |
This register contains a numerical value that is multiplied by the content of the pickup register when Direct Mode is selected. Otherwise, register is not used. The factory setting is 0x8000. |
|
0x1774 |
6005 |
RW |
1 |
s |
INT16U |
– |
H |
Actuation time delay The factory setting is 0x8000. |
|
0x1775 |
6006 |
RW |
– |
– |
INT16U |
– |
H |
Release pick-up value (1) The factory setting is 0x8000. |
|
0x1776 |
6007 |
R |
– |
% |
INT16U |
– |
H |
This register contains a numerical value that is multiplied by the content of the pickup register when Direct Mode is selected. Otherwise, register is not used. The factory setting is 0x8000. |
|
0x1777 |
6008 |
RW |
1 |
s |
INT16U |
0–3000 |
H |
Release time delay. The factory setting is 0x8000. |
|
0x1778 |
6009 |
R |
– |
– |
INT16U |
0–3 |
A/E |
Alarm type: 0 = Over 1 = Under (factory setting) 2 = Equal 3 = Different from 5 is used for all other alarms. |
|
0x1779 |
6010 |
RW |
– |
– |
INT16U |
– |
H |
Action associated with overrunning of the pick-up value after the time delay has run out. Log into the Waveform Capture file (file no. 5). Bit 9 set to 1 = action activated The factory setting is 0. |
|
0x177A |
6011 |
– |
– |
– |
– |
– |
– |
Reserved |
|
(1) When Immediate mode is selected, care must be taken to set this register with the same units and scale factors as the register 6001. (2) No percentage is applied. |
||||||||