DOCA0384EN-01

Modbus Functions

General Description

The Modbus protocol offers a number of functions that are used to read or write data over the Modbus network. The Modbus protocol also offers diagnostic and network-management functions.

Only the Modbus functions handled by the circuit breaker are described here.

Read Functions

The following read functions are available:

Function Code

Subfunction Code

Name

Description

3 (0x03)

Read holding registers

Read n output or internal registers

4 (0x04)

Read input registers

Read n input registers

43 (0x2B)

14 (0x0E)

Read device identification

Read the identification data of the server

43 (0x2B)

15 (0x0F)

Get date and time

Read the date and time of the server

NOTE: Number of registers n is limited to 52 with MasterPacT NT/NW MicroLogic E trip unit.

Read Register Example

The following table shows how to read the rms current on phase 1 (I1) in register 1016 of a MicroLogic Active control unit. The address of register 1016 is 1016 - 1 = 1015 = 0x03F7. The Modbus address of the Modbus server is 1 = 0x01.

Client Request

Server Reply

Field Name

Example

Field Name

Example

Modbus server address

0x01

Modbus server address

0x01

Function code

0x03

Function code

0x03

Address of the register to read (MSB)

0x03

Data length in bytes

0x02

Address of the register to read (LSB)

0xF7

Register value (MSB)

0x02

Number of registers (MSB)

0x00

Register value (LSB)

0x2B

Number of registers (LSB)

0x01

CRC (MSB)

0xNN

CRC (MSB)

0xNN

CRC (LSB)

0xNN

CRC (LSB)

0xNN

The content of register 1016 (address 0x03F7) is 0x022B = 555. Therefore, the rms current on phase 1 (I1) is 555 A.

Set Date and Time Example

The following table shows how to set date and time of a Modbus server. The Modbus address of the Modbus server is 1= 0x01, the new date is October 2, 2025, and the new time is 2:32:03:500 p.m.

NOTE: Use the broadcast mode (with Modbus server address = 0) to set the date and time of all Modbus servers.

Client Request

Server Reply

Field Name

Example

Field Name

Example

Modbus server address

0x01

Modbus server address

0x01

Function code

0x2B

Function code

0x2B

Subfunction code

0x10

Subfunction code

0x10

Reserved1

0x00

Reserved1

0x00

Not used

0x00

Not used

0x00

Year = 2025

0x19

Year = 2025

0x19

Month = October

0x0A

Month = October

0x0A

Day Of Month = 2

0x02

Day Of Month = 2

0x02

Hour = 14

0x0E

Hour = 14

0x0E

Minutes = 32

0x20

Minutes = 32

0x20

3 sec. 500 ms

0x0DAC

3 sec. 502 ms

0x0DAE

The normal response is an echo of the request, returned after the date-time has been updated in the remote device. If the date-time structure content is not consistent with a true date-time (that is, an invalid date-time), the value returned in the Date-Time field is set to 0 by the device.

In case of 24 Vdc power loss, the date and time of the Modbus servers without battery is not refreshed anymore. It is therefore mandatory to set date and time for all Modbus servers after recovering the 24 Vdc power supply.

Furthermore, due to the clock drift of each Modbus server, it is mandatory to set date and time for all Modbus servers periodically. Recommended period is at least every 15 minutes.

Scattered Holding Register Read Function

The scattered holding register read function is available:

Function Code

Subfunction Code

Name

Description

100 (0x64)

4 (0x04)

Read scattered holding register

Read n non-contiguous registers

The maximum value for n is 100, but when using a MasterPacT NT/NW MicroLogic A or E trip unit, it is recommended to have n lower or equal to 21.

The scattered holding register read function enables the user to:

  • avoid reading a large block of contiguous registers when only few registers are needed

  • avoid multiple use of functions 3 and 4 in order to read non-contiguous registers

Read Scattered Holding Register Example

The following table shows how to read the addresses of the register 664 (address 0x0297) and register 666 (address 0x0299) of a Modbus server. The Modbus address of the Modbus server is 1 = 0x01.

Client Request

Server Reply

Field Name

Example

Field Name

Example

Modbus server address

0x01

Modbus server address

0x01

Function code

0x64

Function code

0x64

Data length in bytes

0x06

Data length in bytes

0x06

Subfunction code

0x04

Subfunction code

0x04

Transmission number(1)

0xNN

Transmission number(1)

0xNN

Address of first register to read (MSB)

0x02

Value of the first register read (MSB)

0x12

Address of first register to read (LSB)

0x97

Value of the first register read (LSB)

0x0A

Address of second register to read (MSB)

0x02

Value of the second register read (MSB)

0x74

Address of second register to read (LSB)

0x99

Value of the second register read (LSB)

0x0C

CRC (MSB)

0xNN

CRC (MSB)

0xNN

CRC (LSB)

0xNN

CRC (LSB)

0xNN

(1) The client gives the transmission number in the request. The server returns the same number in the reply.

Write Functions

The following write functions are available:

Function Code

Subfunction Code

Name

Description

6 (0x06)

Preset single register

Write 1 register

16 (0x10)

Preset multiple registers

Write n registers

43 (0x2B)

16 (0x10)

Set date and time

Write the date and time of the server

NOTE: Number of registers n is limited to 52 with MasterPacT NT/NW MicroLogic E trip units.

Diagnostic Functions

The following diagnostic functions are available:

Function Code

Subfunction Code

Name

Description

8 (0x08)

10 (0x0A)

Clear counters and diagnostic register

Reset all diagnostic counters

8 (0x08)

11 (0x0B)

Return bus message counter

Read the counter of correct bus messages managed by the server

8 (0x08)

12 (0x0C)

Return bus communication error counter

Read the counter of incorrect bus messages managed by the server

8 (0x08)

13 (0x0D)

Return bus exception error counter

Read the counter of exception responses managed by the server

8 (0x08)

14 (0x0E)

Return server message counter

Read the counter of messages sent to the server

8 (0x08)

15 (0x0F)

Return server no response counter

Read the counter of broadcast messages

8 (0x08)

16 (0x10)

Return server negative acknowledge counter

Read the counter of messages sent to the server but not answered because of the Negative Acknowledge exception code 07

8 (0x08)

17 (0x11)

Return server busy counter

Read the counter of messages sent to the server but not answered because of the Server Device Busy exception code 06

8 (0x08)

18 (0x12)

Return bus overrun counter

Read the counter of incorrect bus messages due to overrun errors

11 (0x0B)

Get communication event counter

Read Modbus event counter

Diagnostic Counters

Modbus uses diagnostic counters to enable performance and error management. The counters are accessible using the Modbus diagnostic functions (function codes 8 and 11). The Modbus diagnostic counters and the Modbus event counter are described in the following table:

Counter Number

Counter Name

Description

1

Bus message counter

Counter of correct bus messages managed by the server

2

Bus communication error counter

Counter of incorrect bus messages managed by the server

3

Server exception error counter

Counter of exception responses managed by the server and incorrect broadcast messages

4

Server message counter

Counter of messages sent to the server

5

Server no response counter

Counter of broadcast messages

6

Server negative acknowledge counter

Counter of messages sent to the server but not answered because of the Negative Acknowledge exception code 07

7

Server busy count

Counter of messages sent to the server but not answered because of the Server Device Busy exception code 06

8

Bus character overrun counter

Counter of incorrect bus messages due to overrun errors

9

Comm. event counter

Modbus event counter (this counter is read with function code 11)

Counters Reset

The diagnostic counters are reset to 0 when:

  • the maximum value 65535 is reached,

  • they are reset by a Modbus command (function code 8, sub-function code 10),

  • the power supply is lost,

  • the communication parameters are modified.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?