DOCA0384EN-01

Counters

General Description

The BCM ULP module has counters that help managing the circuit breaker.

The BCM ULP module counters have the following properties:

  • All the counters are saved in non-volatile memory to prevent data loss in case of power loss.

  • The cumulating OF counter is read only. It stops incrementing when it reaches the maximum value of 65535.

  • All counters (except the cumulating OF counter) can be preset to any value from 0 to 65535. The counters automatically cycle from 65535 to 0.

  • A threshold is associated to the OF counter and to the close circuit breaker command counter.

    The thresholds can be set to any value from 0 to 65534. The factory setting is 5000. An alarm is generated when a counter reaches the threshold.

BCM ULP Module Counters

Address

Register

RW

X

Unit

Type

Range

A/E/P/H

Description

0x0229

554

R

INT16U

0–65535

A/E/P/H

Counter for the number of times the BCM ULP module is energized

0x022A

555

R

INT16U

0–65535

A/E/P/H

Counter for the number of times the BCM ULP module is reset whether following power loss or not

Counter Thresholds

Address

Register

RW

X

Unit

Type

Range

A/E/P/H

Description

0x0243

580

RW

INT16U

0–65535

A/E/P/H

OF counter threshold

Factory setting = 5000

0x0244

581

RW

INT16U

0–65535

A/E/P/H

Close command counter threshold

Factory setting = 5000

Circuit Breaker Operation Counters

Address

Register

RW

X

Unit

Type

Range

A/E/P/H

Description

0x0295

662

R

INT16

0–65535

A/E/P/H

Cumulating OF counter (non-resettable open to close counter)

0x0296

663

RW

INT16

0–65535

A/E/P/H

OF counter (resettable open to close counter)

0x0297

664

RW

INT16

0–65535

A/E/P/H

SD counter (close to SD position)

0x0298

665

RW

INT16

0–65535

A/E/P/H

SDE counter (close to SDE position)

MX and XF Release Counters

Address

Register

RW

X

Unit

Type

Range

A/E/P/H

Description

0x02A1

674

R

INT16U

0–65535

A/E/P/H

MX actuation counter

0x02A5

678

R

INT16U

0–65535

A/E/P/H

XF actuation counter

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?