Legacy Dataset
Description
The legacy dataset contains the most useful information of each IMU module in one convenient table. The legacy dataset is available in the registers 12000 to 12113. It can be read with one read request.
Each IMU module updates the values in the dataset registers on a regular basis.
The response time of requests to legacy dataset registers is shorter than the response time of requests to device registers. Therefore, it is recommended to read the legacy dataset registers instead of device registers, to improve the overall performance of the system. For more information, refer to Modbus Programming Recommendations.
The legacy dataset can be used with:
-
the IFE Ethernet communication interface for one circuit breaker
-
the IFE Ethernet switchboard server
-
the EIFE embedded Ethernet interface for MasterPacT MTZ drawout circuit breaker
-
the IFM Modbus SL communication interface for one circuit breaker
-
the BSCM Modbus SL/ULP module
-
The legacy dataset is compatible with legacy versions of the MicroLogic trip unit for ComPacT NSX, PowerPacT H-, J-, and L-Frame, ComPacT NS, PowerPacT P- and R-frame or MasterPacT NT/NW circuit breaker. For this reason, data read directly in the Modbus registers is organized in a different way than in the standard dataset.
-
For new applications, it is recommended to use the standard dataset instead of the legacy dataset.
Legacy Dataset for MicroLogic X Control Units
The legacy dataset is available when the Modbus legacy dataset Digital Module is purchased and installed on a MicroLogic X control unit.
The Modbus legacy dataset Digital Module is compatible with MicroLogic X control units with firmware version greater than or equal to version V002.000.nnn.
The Modbus legacy dataset is available on a remote controller using the communication network through the following communication interfaces:
-
IFE Ethernet interface
-
EIFE Ethernet interface
-
IFE server
-
IFM Modbus-SL interface
The following table shows the part numbers and firmware versions necessary to access the Modbus legacy dataset through communication interfaces:
|
Communication interface |
Part number |
Minimum firmware version required |
|---|---|---|
|
IFE Ethernet interface |
LV434010 |
V003.007.024 |
|
LV434001 |
||
|
IFE server |
LV434011 |
V003.007.024 |
|
LV434002 |
||
|
EIFE Ethernet interface |
LV851001 |
V003.007.024 |
|
IFM Modbus-SL interface |
LV434000 |
V003.001.006 |