DOCA0384EN-01

Generic Commands

Change Output State

The command is used to change the state of IO module digital outputs assigned as user-defined outputs using EcoStruxure Power Commission software.

To change the output state, set the command registers as follows:

Address

Register

Unit

Type

Range

Description

0x1F3F

8000

INT16U

1672

Command code = 1672

0x1F40

8001

INT16U

13

Number of parameters (bytes) = 13

0x1F41

8002

INT16U

Destination =

  • IO 1: 8193 (0x2001)

  • IO 2: 8449 (0x2101)

0x1F42

8003

INT16U

1

Security type of the command

0x1F43–0x1F44

8004–8005

OCTET STRING

Password of the command: Administrator or Operator user profile password

0x1F45

8006

INT16U

1–3

Output number

  • 1 = output 1

  • 2 = output 2

  • 3 = output 3

0x1F46

8007

INT16U

Value to set:

  • 0x0000 = Change output state to 0 (OFF)

  • 0x0100 = Change output state to 1 (ON)

Reset IO Module Alarm

The alarms can be read from the alarm status register.

To reset IO module alarms, set the command registers as follows:

Address

Register

Unit

Type

Range

Description

0x1F3F

8000

INT16U

41099

Command code = 41099

0x1F40

8001

INT16U

10

Number of parameters (bytes) = 10

0x1F41

8002

INT16U

Destination =

  • IO 1: 8193 (0x2001)

  • IO 2: 8449 (0x2101)

0x1F42

8003

INT16U

1

Security type of the command

0x1F43–0x1F44

8004–8005

OCTET STRING

Password of the command: Administrator or Operator user profile password

Enable/Disable Simple Commands

To enable or disable the simple commands, set the command registers as follows:

Address

Register

Unit

Type

Range

Description

0x1F3F

8000

INT16U

41100

Command code = 41100

0x1F40

8001

INT16U

11

Number of parameters (bytes) = 11

0x1F41

8002

INT16U

Destination =

  • IO 1: 8193 (0x2001)

  • IO 2: 8449 (0x2101)

0x1F42

8003

INT16U

1

Security type of the command

0x1F43–0x1F44

8004–8005

OCTET STRING

Password of the command: Administrator or Operator user profile password

0x1F45

8006

INT16U

MSB: Enable or disable:

  • 0 = Disable simple command

  • 1 = Enable simple command

LSB: 0 (not used)

Acknowledge Latched Output

To acknowledge the latched output, set the command registers as follows:

Address

Register

Unit

Type

Range

Description

0x1F3F

8000

INT16U

41102

Command code = 41102

0x1F40

8001

INT16U

11

Number of parameters (bytes) = 11

0x1F41

8002

INT16U

Destination =

  • IO 1: 8193 (0x2001)

  • IO 2: 8449 (0x2101)

0x1F42

8003

INT16U

1

Security type of the command

0x1F43–0x1F44

8004–8005

OCTET STRING

Password of the command: Administrator or Operator user profile password

0x1F45

8006

INT16U

MSB:

  • 0x01 = Digital output relay 1

  • 0x02 = Digital output relay 2

  • 0x03 = Digital output relay 3

  • 0xFF = Unlatch all digital output

LSB: 0 (not used)

Reset Analog Input Minimum/Maximum Values

The analog input maximum and minimum values can be read from the analog input registers.

To reset the minimum/maximum analog input values, set the command registers as follows:

Address

Register

Unit

Type

Range

Description

0x1F3F

8000

INT16U

42890

Command code = 42890

0x1F40

8001

INT16U

10

Number of parameters (bytes) = 10

0x1F41

8002

INT16U

Destination =

  • IO 1: 8193 (0x2001)

  • IO 2: 8449 (0x2101)

0x1F42

8003

INT16U

1

Security type of the command

0x1F43–0x1F44

8004–8005

OCTET STRING

Password of the command: Administrator or Operator user profile password

Get Events Command

To get events, set the command registers in the following way:

Address

Register

Unit

Type

Range

Bit

Description

0x1F3F

8000

INT16U

50560

Command code = 50560

0x1F40

8001

INT16U

27

Number of parameters (bytes) = 27

0x1F41

8002

INT16U

Destination =

  • IO 1: 8193 (0x2001)

  • IO 2: 8449 (0x2101)

0x1F42

8003

INT16U

0

Security type of the command

0x1F43–0x1F44

8004–

8005

OCTET STRING

Password of the command = 0 (no password required)

0x1F45

8006

Reserved

0x1F46

8007

INT16U

0, 2

Requested get event method:

  • 0 = Most recent events

  • 2 = Events before and up to a sequence number

0x1F47–0x1F4A

8008–8011

Reserved

0x1F4B–0x1F4C

8012–8013

INT32U

Requested event sequence number (for method 2 only)

0x1F4D

8014

INT16U

Requested event severity

0–7

Reserved

8

Low

9

Medium

10

High

11–15

Reserved

Events are returned to command registers in the following way:

Address

Register

Unit

Type

Range

Bit

Description

0x1F53

8020

INT16U

50560

Last command code

0x1F54

8021

INT16U

Command status:

0x1F55

8022

INT16U

Number of bytes returned

0x1F56

8023

Reserved

0x1F57

8024

INT16U

0, 2

Responded get event method:

  • 0 = Most recent events

  • 2 = Events before and up to a sequence number

0x1F5E

8031

INT16U

Responded event severity

0–7

Reserved

8

Low

9

Medium

10

High

11–15

Reserved

0x1F5F

8032

INT16U

MSB: Number of events returned

LSB: Remaining events

  • 0 = No more events to get

  • 1 = More events to get

0x1F60

8033

INT16U

1013-25630

First event code

0x1F61–0x1F64

8034–8037

DATETIME

Timestamp of the first event

0x1F65

8038

INT16U

Timestamp quality of the first event

0x1F66–0x1F67

8039–8040

INT32U

First event sequence number

0x1F68

8041

INT16U

MSB: First event status

  • 1 = Occurrence

  • 2 = Completion

  • 3 = Pulse

LSB: Reserved

0x1F69

8042

Reserved

0x1F6A

8043

INT16U

First event severity

0–7

Reserved

8

Low

9

Medium

10

High

11–15

Reserved

0x1F6B–0x1F75

8044–8054

INT16U

Characteristics of event 2 (same as event 1)

0x1F76–0x1F80

8055–8065

INT16U

Characteristics of event 3 (same as event 1)

0x1F81– 0x1F8B

8066–8076

INT16U

Characteristics of event 4 (same as event 1)

0x1F8C–0x1F96

8077–8087

INT16U

Characteristics of event 5 (same as event 1)

0x1F97–0x1FA1

8088–8098

INT16U

Characteristics of event 6 (same as event 1)

0x1FA2–0x1FAC

8099–8109

INT16U

Characteristics of event 7 (same as event 1)

0x1FAD–0x1FB7

8110–8120

INT16U

Characteristics of event 8 (same as event 1)

0x1FB8–0x1FC2

8121–8131

INT16U

Characteristics of event 9 (same as event 1)

0x1FC3–0x1FCD

8132–8142

INT16U

Characteristics of event 10 (same as event 1)

Get Events Procedure

The command allows to get events by using one of the two following methods:

  • get the most recent events

  • get events before and up to an event sequence number. The event sequence number is an event identifier defined by the device, and is available among the event characteristics. It can be used to sort the events in chronological order.

The command allows to get 10 events maximum for one or several severity levels.

  • To get the 10 most recent events, use the method “get the most recent events”.

  • If there are more than 10 events, use the other method “get events before and up to an event sequence number” to get rest of the events.

Example: Read all events:

The following diagram shows the steps to follow to read all events recorded in the device:

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?