DOCA0384EN-01

Reset Minimum/Maximum Commands

Reset Minimum/Maximum

The reset minimum/maximum command resets the minimum values of real-time measurements (registers 1300 to 1599) and the maximum values of real-time measurements (registers 1600 to 1899).

The reset minimum/maximum command resets the energy measurements (registers 2000 to 2027).

The reset minimum/maximum command resets the peak demand measurements (registers 2200 to 2241).

To reset minimum/maximum values of measurements, the user must set up the command registers as follows:

Address

Register

X

Unit

Type

Range

A/E

Bit

Description

0x1F3F

8000

INT16U

46728

Command code = 46728

0x1F40

8001

INT16U

12

Number of parameters (bytes) = 12

0x1F41

8002

INT16U

4609

Destination = 4609 (0x1201)

0x1F42

8003

INT16U

1

Security type of the command

0x1F43–0x1F44

8004–8005

OCTET STRING

Password of the command: Administrator or Operator user profile password

0x1F45

8006

INT16U

Reset minimum/maximum of metering variables:

  • To reset the metering variable, set the bit to 1.

  • To keep the current values, set the bit to 0.

A/E

0

Reset minimum/maximum current (I1, I2, I3, IN, Imax, Ig, Iavg, and Iunbal)

E

1

Reset minimum/maximum voltage (V12, V13, V23, V1N, V2N, V3N, VavgL-L, VavgL-N, and Vunbal)

E

2

Reset minimum/maximum power (active power, reactive power, apparent power, and distortion power)

E

3

Reset minimum/maximum power factor and cosϕ

4

Reserved

E

5

Reset peak of current demand

E

6

Reset peak of active power, reactive power, and apparent power demand

E

7

Reset minimum/maximum frequency

8

Reserved

E

9

Reset energy (active, reactive, apparent)

10–15

Reserved

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.