DOCA0384EN-01

Counters

General Description

The MicroLogic Active control unit has counters which are used to manage the circuit breaker.

The MicroLogic Active counters have the following properties:

  • All the counters are saved in non-volatile memory to prevent data loss in case of power loss.

  • The cumulating OF counter is read only. It stops incrementing when it reaches the maximum value of 65535.

  • A threshold is associated to the OF counter. An alarm is generated when a counter reaches the threshold.

Counter Thresholds

Address

Register

RW

X

Unit

Type

Range

A/E

Description

0x0243

580

R

INT16U

0–65535

A/E

OF counter threshold

Factory setting = 5000

Circuit Breaker Operation Counters

Address

Register

RW

X

Unit

Type

Range

A/E

Description

0x0296

663

R

INT16

0–65535

A/E

OF counter (resettable open to close counter)

0x0297

664

R

INT16

0–65535

A/E

SD counter (close to SD position)

0x0298

665

R

INT16

0–65535

A/E

SDE counter (close to SDE position)

MX and XF Release Counters

Address

Register

RW

X

Unit

Type

Range

A/E

Description

0x02A1

674

R

INT16U

0–65535

A/E

MX actuation counter

0x02A2–0x02A4

675–677

Reserved

0x02A5

678

R

INT16U

0–65535

A/E

XF actuation counter

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.