DOCA0384EN-01

Waveform Capture

General Description

The system stores the variables V1N, V2N, V3N, I1, I2, I3, IN during four cycles (64 points per cycles) in the file number 5.

This file consists of a fixed number of records (29). All records are of similar size that is 64 registers wide.

The capture is triggered as follows:

File Header

The following table describes the file header content:

Address

Register

RW

X

Unit

Type

Range

A/E/P/H

Description

0x1BDB

7132

RW

INT16U

H

File status:

0x0000 = file disabled

0xFFFF = file enabled (factory setting)

0x1BDC

7133

R

INT16U

H

Type of file:

5 = waveform capture

0x1BDD

7134

R

1

INT16U

H

Size of a file = 29 records

0x1BDE

7135

R

1

INT16U

H

Size of a record = 64 registers

0x1BDF

7136

R

INT16U

1

H

File filling mode:

0 = circular

1 = disabled if log is full

0x1BE0

7137

R

1

INT16U

H

Number of cycle segments:

1 = 4 cycles for waveform capture

0x1BE1

7138

R

1

INT16U

H

Number of cycles before capture:

2 = waveform capture and fault waveform capture

0x1BE2

7139

R

1

INT16U

H

Number of points per cycle:

64 = waveform capture

File Status

The following table describes the file status content:

Address

Register

RW

X

Unit

Type

Range

A/E/P/H

Description

0x1BEB

7148

R

1

INT16U

H

Size of a file = 29 records

0x1BEC

7149

R

1

INT16U

H

Size of a record = 64 registers

0x1BED

7150

R

1

INT16U

H

0x0000 = file OK

0x000A = record size smaller than expected

0x0014 = record size larger than expected

0x001E = insufficient memory

0x00FA = internal error

0x00FD = corrupted allocation table

0x00FE = configuration zero

0x00FF = invalid configuration

0xFC00 = invalid file number

0xFD00 = invalid record number

0xFE00 = file not supported

0xFF00 = cannot allocate file

0x1BEE

7151

R

1

INT16U

H

Number of records in the file = 29

0x1BEF

7152

R

1

INT16U

H

Sequence number of first record in the file (the oldest) = 1

0x1BF0

7153

R

1

INT16U

H

Sequence number of last record in the file (the most recent) = 29

0x1BF1– 0x1BF3

7154– 7156

R

DATE

H

Date the last file was reset.

Factory setting = 0x8000 0x8000 0x8000

Waveform Record

The waveform capture has a fixed number of records and all record has a fixed number of registers:

Record Number

Registers

Type

Description

1

1–4

XDATE

Extended date/time

5–11

Reserved

12

INT16U

ID of fault WFC trigger: Alarm number 1000 to 1031

13

System type: 31, 40 or 41

14

A

Circuit breaker nominal current

15

SFIXPT

Voltage multiplier for phase 1

16

INT16

Voltage offset for phase 1

17

SFIXPT

Voltage multiplier for phase 2

18

INT16

Voltage offset for phase 2

19

SFIXPT

Voltage multiplier for phase 3

20

INT16

Voltage offset for phase 3

21

SFIXPT

Current multiplier for phase 1

22

INT16

Current offset for phase 1

23

SFIXPT

Current multiplier for phase 2

24

INT16

Current offset for phase 2

25

SFIXPT

Current multiplier for phase 3

26

INT16

Current offset for phase 3

27

SFIXPT

Current multiplier for neutral

28

INT16

Current offset for neutral

29

INT16U

Scaling factor used for SFIXPT math on voltage samples

30

INT16U

Scaling factor used for SFIXPT math on phase-current samples

31

INT16U

Scaling factor used for SFIXPT math on neutral-current samples

32–64

Not used

2–4

1–64

INT16U

Voltage V1N sample points (16 points - 12 cycles)

5–7

1–64

INT16U

Voltage V2N sample points (16 points - 12 cycles)

8–10

1–64

INT16U

Voltage V3N sample points (16 points - 12 cycles)

11–13

1–64

INT16U

Current I1 sample points (16 points - 12 cycles)

14–16

1–64

INT16U

Current I2 sample points (16 points - 12 cycles)

17–19

1–64

INT16U

Current I3 sample points (16 points - 12 cycles)

20–22

1–64

INT16U

Current IN sample points (16 points - 12 cycles)

Valid only with system type 41

Voltage Calculation

Apply the following rules to derive the voltages:

  • on phase 1:

    Sample (Volt) = [(sample – mean value of Voltage V1N sample points) x register number 15 of first record]/(1000 x register number 29 of first record).

  • on phase 2:

    Sample (Volt) = [(sample – mean value of Voltage V2N sample points) x register number 17 of first record]/(1000 x register number 29 of first record).

  • on phase 3:

    Sample (Volt) = [(sample – mean value of Voltage V3N sample points) x register number 19 of first record]/(1000 x register number 29 of first record).

Current Calculation

Apply the following rules to derive the currents:

  • on phase 1:

    Sample (Ampere) = [(sample – mean value of Current I1 sample points) x register number 21 of first record] / ((1000 x register number 30 of first record) / Circuit breaker nominal current).

  • on phase 2:

    Sample (Ampere) = [(sample – mean value of Current I2 sample points) x register number 23 of first record] / ((1000 x register number 30 of first record) / Circuit breaker nominal current).

  • on phase 3:

    Sample (Ampere) = [(sample – mean value of Current I3 sample points) x register number 25 of first record] / ((1000 x register number 30 of first record) / Circuit breaker nominal current).

  • on neutral:

    Sample (Ampere) = [(sample – mean value of Current IN sample points) x register number 27 of first record] / ((1000 x register number 31 of first record) / Circuit breaker nominal current).

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?