Fault Waveform Capture
General Description
The system stores the variables V1N, V2N, V3N, I1, I2, I3, IN during 12 cycles (16 points per cycles) in the file number 22.
This file consists of a fixed number of records (22). All records are of similar size that is 64 registers wide.
The capture is triggered automatically attached to alarms (1000–1030) by setting the log action to 1.
File Header
The following table describes the file header content:
|
Address |
Register |
RW |
X |
Unit |
Type |
Range |
A/E/P/H |
Description |
|---|---|---|---|---|---|---|---|---|
|
0x26EB |
9964 |
RW |
– |
– |
INT16U |
– |
H |
File status: 0x0000 = file disabled 0xFFFF = file enabled (factory setting) |
|
0x26EC |
9965 |
R |
– |
– |
INT16U |
– |
H |
Type of file: 22 = fault waveform capture |
|
0x26ED |
9966 |
R |
1 |
– |
INT16U |
– |
H |
Size of a file = 22 records |
|
0x26EE |
9967 |
R |
1 |
– |
INT16U |
– |
H |
Size of a record = 64 registers |
|
0x26EF |
9968 |
R |
– |
– |
INT16U |
1 |
H |
File filling mode: 0 = circular 1 = disabled if log is full |
|
0x26F0 |
9969 |
R |
1 |
– |
INT16U |
– |
H |
Number of cycle segments: 1 = 12 cycles for fault waveform capture |
|
0x26F1 |
9970 |
R |
1 |
– |
INT16U |
– |
H |
Number of cycles before capture: 2 = waveform capture and fault waveform capture |
|
0x26F2 |
9971 |
R |
1 |
– |
INT16U |
– |
H |
Number of points per cycle: 16 = fault waveform capture |
File Status
The following table describes the file status content:
|
Address |
Register |
RW |
X |
Unit |
Type |
Range |
A/E/P/H |
Description |
|---|---|---|---|---|---|---|---|---|
|
0x26FB |
9980 |
R |
1 |
– |
INT16U |
– |
H |
Size of a file = 22 records |
|
0x26FC |
9981 |
R |
1 |
– |
INT16U |
– |
H |
Size of a record = 64 registers |
|
0x26FD |
9982 |
R |
1 |
– |
INT16U |
– |
H |
0x0000 = file OK 0x000A = record size smaller than expected 0x0014 = record size larger than expected 0x001E = insufficient memory 0x00FA = internal error 0x00FD = corrupted allocation table 0x00FE = configuration zero 0x00FF = invalid configuration 0xFC00 = invalid file number 0xFD00 = invalid record number 0xFE00 = file not supported 0xFF00 = cannot allocate file |
|
0x26FE |
9983 |
R |
1 |
– |
INT16U |
– |
H |
Number of records in the file = 22 |
|
0x26FF |
9984 |
R |
1 |
– |
INT16U |
– |
P/H |
Sequence number of first record in the file (the oldest) = 1 |
|
0x2700 |
9985 |
R |
1 |
– |
INT16U |
– |
P/H |
Sequence number of last record in the file (the most recent) = 22 |
|
0x2701– 0x2703 |
9986– 9988 |
R |
– |
– |
DATE |
– |
H |
Date the last file was reset. Factory setting = 0x8000 0x8000 0x8000 |
Fault Waveform Record
The fault waveform capture has a fixed number of records and all record has a fixed number of registers:
|
Record Number |
Registers |
Type |
Description |
|---|---|---|---|
|
1 |
1–4 |
XDATE |
Extended date/time |
|
5–11 |
– |
Reserved |
|
|
12 |
INT16U |
||
|
13 |
– |
||
|
14 |
A |
Circuit breaker nominal current |
|
|
15 |
SFIXPT |
Voltage multiplier for phase 1 |
|
|
16 |
INT16 |
Voltage offset for phase 1 |
|
|
17 |
SFIXPT |
Voltage multiplier for phase 2 |
|
|
18 |
INT16 |
Voltage offset for phase 2 |
|
|
19 |
SFIXPT |
Voltage multiplier for phase 3 |
|
|
20 |
INT16 |
Voltage offset for phase 3 |
|
|
21 |
SFIXPT |
Current multiplier for phase 1 |
|
|
22 |
INT16 |
Current offset for phase 1 |
|
|
23 |
SFIXPT |
Current multiplier for phase 2 |
|
|
24 |
INT16 |
Current offset for phase 2 |
|
|
25 |
SFIXPT |
Current multiplier for phase 3 |
|
|
26 |
INT16 |
Current offset for phase 3 |
|
|
27 |
SFIXPT |
Current multiplier for neutral |
|
|
28 |
INT16 |
Current offset for neutral |
|
|
29 |
INT16U |
Scaling factor used for SFIXPT math on voltage samples |
|
|
30 |
INT16U |
Scaling factor used for SFIXPT math on phase current samples |
|
|
31 |
INT16U |
Scaling factor used for SFIXPT math on neutral current samples |
|
|
32–64 |
– |
Not used |
|
|
2–4 |
1–64 |
INT16U |
Voltage V1N sample points (16 points - 12 cycles) |
|
5–7 |
1–64 |
INT16U |
Voltage V2N sample points (16 points - 12 cycles) |
|
8–10 |
1–64 |
INT16U |
Voltage V3N sample points (16 points - 12 cycles) |
|
11–13 |
1–64 |
INT16U |
Current I1 sample points (16 points - 12 cycles) |
|
14–16 |
1–64 |
INT16U |
Current I2 sample points (16 points - 12 cycles) |
|
17–19 |
1–64 |
INT16U |
Current I3 sample points (16 points - 12 cycles) |
|
20–22 |
1–64 |
INT16U |
Current IN sample points (16 points - 12 cycles) Valid only with system type 41 |
Voltage Calculation
Apply the following rules to derive the voltages:
-
on phase 1:
Sample (Volt) = [(sample – register number 16 of first record) x register number 15 of first record.]/register number 29 of first record.
-
on phase 2:
Sample (Volt) = [(sample – register number 18 of first record) x register number 17 of first record.]/register number 29 of first record.
-
on phase 3:
Sample (Volt) = [(sample – register number 20 of first record) x register number 19 of first record.]/register number 29 of first record.
Current Calculation
Apply the following rules to derive the currents:
-
on phase 1:
Sample (Ampere) = [(sample – register number 22 of first record) x register number 21 of first record.]/register number 30 of first record.
-
on phase 2:
Sample (Ampere) = [(sample – register number 24 of first record) x register number 23 of first record.]/register number 30 of first record.
-
on phase 3:
Sample (Ampere) = [(sample – register number 26 of first record) x register number 25 of first record.]/register number 30 of first record.
-
on neutral:
Sample (Ampere) = [(sample – register numbr 27 of first record) x register number 28 of first record.]/register number 31 of first record.