DOCA0384EN-01

List of MicroLogic Active Commands and Error Codes

List of Commands

The following table lists the available MicroLogic Active control unit commands, their corresponding command codes, and user profiles. Follow the command execution procedures.

Command

Command Code

User Profile

Open circuit breaker

904

No password required

Close circuit breaker

905

No password required

Reset minimum/maximum

46728

No password required

Error Codes

Error codes generated by MicroLogic Active control units are the generic error codes.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?