DOCA0384EN-01

Minimum/Maximum Values of Real-Time Measurements

Minimum/Maximum Measurements Rule

Minimum and maximum measurements take into account the relative value of real-time measurements. Therefore the following rule applies:

-3800<-400<0<200<600.

In this case:

  • the minimum value = -3800

  • the maximum value = 600

NOTE: This rule does not apply for the power factor (PF) and for the fundamental power factor (cosϕ):
  • PFmax (or cosϕ max.) is obtained for the smallest positive value of PF (or cosϕ).

  • PFmin (or cosϕ min.) is obtained for the highest negative value of PF (or cosϕ).

The reset minimum/maximum command (command code = 46728) can reset the content of the minimum/maximum real-time measurement registers.

Minimum of Real-Time Measurements

Registers 1300 to 1599 hold the minimum values of real-time metering parameters:

  • Available only with MicroLogic E,P, and H trip units.

  • The register of the minimum value of a real-time metering parameter is equal to the register of the real-time metering parameter plus 300.

    Examples:

    • Register 1300 holds the minimum value of the phase-to-phase voltage V12 (register 1000).

    • Register 1316 holds the minimum value of the current on phase 1 (register 1016).

  • The order of the registers is the same as that of the real-time metering variables.

  • The scale factors of the minimum values are the same as those of the real-time metering parameters.

  • The minimum values of arithmetic means and unbalance voltage (registers 1306–1315) and for unbalance current (registers 1327 to 1332) are not available with MicroLogic E trip units.

Maximum of Real-Time Measurements

Registers 1600 to 1899 hold the maximum values of real-time metering parameters:

  • Available only with MicroLogic E,P, and H trip units.

  • The register of the maximum value of a real-time metering parameter is equal to the register of the real-time metering parameter plus 600.

    Examples:

    • Register 1600 holds the maximum value of the phase-to-phase voltage V12 (register 1000).

    • Register 1616 holds the maximum value of the current on phase 1 (register 1016).

  • The order of the registers is the same as that of the real-time metering variables.

  • The scale factors of the maximum values are the same as those of the real-time metering parameters.

  • The maximum values of arithmetic means and unbalance voltage (registers 1606–1615) and for unbalance current (registers 1627 to 1632) are not available with MicroLogic E trip units.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?