DOCA0384EN-01

Demand Measurements

General Description

Demand registers include:

  • current demand

  • active, reactive, and apparent power demand

The window duration of current demand depends on the configuration of register 3352. Refer to Demand Time.

The window duration and the window type of power demand depend on the configuration of registers 3354 and 3355. Refer to Demand Time.

  • For the block window, the demand value is updated at the end of the window.

  • For the sliding window,

    • If window duration is configured for less or equal to 15 minutes, the demand value is updated every 15 seconds.

    • If window duration is configured for more than 15 minutes, the demand value is updated every 1 minute.

The reset minimum/maximum command (command code = 46728) can reset the content of the peak demand measurement registers.

Current Demand

Address

Register

RW

X

Unit

Type

Range

A/E/P/H

Description

0x0897

2200

R

1

A

INT16U

0–32767

E/P/H

Current demand on phase 1: I1 Dmd (2)

0x0898

2201

R

1

A

INT16U

0–32767

E/P/H

Current demand on phase 2: I2 Dmd (2)

0x0899

2202

R

1

A

INT16U

0–32767

E/P/H

Current demand on phase 3: I3 Dmd (2)

0x089A

2203

R

1

A

INT16U

0–32767

E/P/H

Current demand on the neutral: IN Dmd (1) (2)

0x089B

2204

R

1

A

INT16U

0–32767

E/P/H

Maximum current demand on phase 1 since the last reset: I1 Peak Dmd

0x089C

2205

R

1

A

INT16U

0–32767

E/P/H

Maximum current demand on phase 2 since the last reset: I2 Peak Dmd

0x089D

2206

R

1

A

INT16U

0–32767

E/P/H

Maximum current demand on phase 3 since the last reset: I3 Peak Dmd

0x089E

2207

R

1

A

INT16U

0–32767

E/P/H

Maximum current demand on the neutral since the last reset: IN Peak Dmd (1)

(1) Value is not available when the system type in register 3314 is 31 or 40. Refer to System Type.

(2) Only the thermal algorithm is available with MicroLogic E trip units while MicroLogic P/H trip units have both the thermal and arithmetical mean algorithms.

K-Factor Demand

Address

Register

RW

X

Unit

Type

Range

A/E/P/H

Description

0x08A3

2212

R

10

INT16U

0–1000

H

K-factor demand on phase 1

0x08A4

2213

R

10

INT16U

0–1000

H

K-factor demand on phase 2

0x08A5

2214

R

10

INT16U

0–1000

H

K-factor demand on phase 3

0x08A6

2215

R

10

INT16U

0–1000

H

K-factor demand on the neutral (1)

0x08A7

2216

R

10

INT16U

0–1000

H

Maximum K-factor demand on phase 1 since last reset

0x08A8

2217

R

10

INT16U

0–1000

H

Maximum K-factor demand on phase 2 since last reset

0x08A9

2218

R

10

INT16U

0–1000

H

Maximum K-factor demand on phase 3 since last reset

0x08AA

2219

R

10

INT16U

0–1000

H

Maximum K-factor demand on the neutral since last reset (1)

(1) Value is not available when the system type in register 3314 is 31 or 40. Refer to System Type.

Active Power Demand

Address

Register

RW

X

Unit

Type

Range

A/E/P/H

Description

0x08AF

2224

R

1

kW

INT16U

0–32767

E/P/H

Total active power demand: P Dmd (1) (3)

0x08B0

2225

R

1

kW

INT16U

0–32767

E/P/H

Maximum total active power demand since the last reset: P Peak Dmd

0x08B1

2226

R

1

kW

INT16U

0–32767

P/H

Predicted active power demand at the end of the window (2)

0x08B2

2227

R

1000

INT16

-1000–+1000

P/H

Total power factor at last active power demand maximum

0x08B3

2228

R

1

kvar

INT16U

0–32767

P/H

Reactive power demand at last active power demand maximum

0x08B4

2229

R

1

kVA

INT16U

0–32767

P/H

Apparent power demand at last active power demand maximum

(1) For the block window type, this value is updated at the end of the window interval. For the sliding window type, the value is updated every 15 seconds.

(2) Value is updated every 15 seconds for both block window and sliding window types.

(3) Only the thermal algorithm is available with MicroLogic E trip units while MicroLogic P/H trip units have both the thermal and arithmetical mean algorithms.

Reactive Power Demand

Address

Register

RW

X

Unit

Type

Range

A/E/P/H

Description

0x08B5

2230

R

1

kvar

INT16U

0–32767

P/H

Total reactive power demand: Q Dmd (1)

0x08B6

2231

R

1

kvar

INT16U

0–32767

P/H

Reactive power demand maximum since the last reset: Q Peak Dmd

0x08B7

2232

R

1

kvar

INT16U

0–32767

P/H

Predicted reactive power demand at the end of the window (2)

0x08B8

2233

R

1000

INT16

-1000–+1000

P/H

Total power factor at last reactive power demand maximum

0x08B9

2234

R

1

kW

INT16U

0–32767

P/H

Active power demand at last reactive power demand maximum

0x08BA

2235

R

1

kVA

INT16U

0–32767

P/H

Apparent power demand at last reactive power demand maximum

(1) For the block window type, this value is updated at the end of the window interval. For the sliding window type, the value is updated every 15 seconds.

(2) Value is updated every 15 seconds for both block window and sliding window types.

Apparent Power Demand

Address

Register

RW

X

Unit

Type

Range

A/E/P/H

Description

0x08BB

2236

R

1

kVA

INT16U

0–32767

E/P/H

Total apparent power demand: S Dmd (1)

0x08BC

2237

R

1

kVA

INT16U

0–32767

E/P/H

Maximum total apparent power demand since last reset: S Peak Dmd

0x08BD

2238

R

1

kVA

INT16U

0–32767

P/H

Predicted apparent power demand at the end of the window (2)

0x08BE

2239

R

1000

INT16

-1000–+1000

P/H

Total power factor at last apparent power demand maximum

0x08BF

2240

R

1

kW

INT16U

0–32767

P/H

Active power demand at last apparent power demand maximum

0x08C0

2241

R

1

kvar

INT16U

0–32767

P/H

Reactive power demand at last apparent power demand maximum

(1) For the block window type, this value is updated at the end of the window interval. For the sliding window type, the value is updated every 15 seconds.

(2) Value is updated every 15 seconds for both block window and sliding window types.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?