DOCA0384EN-01

Minimum/Maximum Measurements Reset Time

Overview

The minimum/maximum measurements reset time registers enable the user to know all the dates relative to the last reset minimum/maximum command.

The reset minimum/maximum command (command code 46728) can reset the content of the minimum/maximum measurements registers.

A read request of 30 registers is necessary to read the minimum/maximum measurements reset time.

Minimum/Maximum Measurements Reset Time

Address

Register

RW

X

Unit

Type

Range

Description

0x0B53–

0x0B55

2900–

2902

R

ULP DATE

Date and time of reset of minimum/maximum current Data Type: ULP DATE

0x0B56–

0x0B58

2903–

2905

R

ULP DATE

Date and time of reset of minimum/maximum voltage.

0x0B59–

0x0B5B

2906–

2908

R

ULP DATE

Date and time of reset of minimum/maximum power (P, Q, S).

0x0B5C–

0x0B5E

2909–

2911

R

ULP DATE

Date and time of reset of minimum/maximum power factor and cosϕ.

0x0B5F–

0x0B61

2912–

2914

R

ULP DATE

Date and time of reset of minimum/maximum total harmonic distortion.

0x0B62–

0x0B64

2915–

2917

R

ULP DATE

Date and time of reset of peak current demand.

0x0B65–

0x0B67

2918–

2920

R

ULP DATE

Date and time of reset of peak active, reactive, and apparent power demand.

0x0B68–

0x0B6A

2921–

2923

R

ULP DATE

Date and time of reset of minimum/maximum frequency.

0x0B6B–

0x0B6D

2924–

2926

R

ULP DATE

Date and time of reset of minimum/maximum thermal image of motor.

0x0B6E–

0x0B70

2927–

2929

R

ULP DATE

Date and time of reset of energy (active, reactive, and apparent).

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?