Password Management
General Description
Remote access to data on MicroLogic trip units and control units, and the ULP modules of the IMU is protected by password. Remote access includes:
-
The communication network
-
EcoStruxure Power Commission software
-
EcoStruxure Power Device App
-
FDM128 display
-
IFE/EIFE webpages
The following four profiles are defined for remote access. Each IMU has a different password for each user profile.
-
Administrator
-
Services
-
Engineer
-
Operator
The Administrator password is required to write the settings to the MicroLogic trip unit or control unit, and the ULP modules of the IMU using EcoStruxure Power Commission software.
Each intrusive command via the command interface is assigned to one or several user profiles, and protected by the corresponding user profile password. The password for each intrusive command is indicated in the description of the command.
-
Remote protection setting commands are allowed only when the Remote Settings parameter of MicroLogic Active control unit is set to ON.
-
Remote open/close commands from an FDM121 display are allowed only when MicroLogic Active control unit is in Auto Local control mode.
-
Remote open/close commands from a remote monitoring and control interface are allowed only when MicroLogic Active control unit is in Auto Remote control mode.
-
Remote open/close commands are not allowed when MicroLogic Active control unit is in Manual control mode.
No password is required for non-intrusive commands through the command interface.
Default Passwords
WARNING |
|---|
|
POTENTIAL COMPROMISE OF SYSTEM AVAILABILITY, INTEGRITY,
AND CONFIDENTIALITY
Change default passwords at first use to help prevent
unauthorized access to device settings, controls, and information.
Failure to follow these instructions can result in death, serious injury, or equipment
damage.
|
The default password for each user profile is as follows:
|
User profile |
Default password |
|---|---|
|
Administrator |
‘0000’ = 0x30303030 |
|
Services |
‘1111’ = 0x31313131 |
|
Engineer |
‘2222’ = 0x32323232 |
|
Operator |
‘3333’ = 0x33333333 |
Changing a Password
A password can be changed with EcoStruxure Power Commission software.
Entering the current password for a given user profile is required to change the password of this user profile. Entering the Administrator password enables you to change the password of any user profile.
A password is composed of exactly 4 ASCII characters. It is case-sensitive and the allowed characters are:
-
Digits from 0 to 9
-
Letters from a to z
-
Letters from A to Z
Passwords of the IMU
The MicroLogic trip unit or control unit, and the ULP modules of the IMU must be protected by the same password for each user profile.
When using EcoStruxure Power Commission software to modify a password, the password is modified in the MicroLogic trip unit or control unit, and the ULP modules of the IMU.
It is compulsory to assign the current IMU passwords to a new module in the IMU, in case of:
-
addition of a new ULP module in the IMU.
-
replacement of the MicroLogic trip unit or control unit, or one of the ULP modules of the IMU.
Use EcoStruxure Power Commission software to modify the passwords of the new module to match the current IMU passwords.
Example: Addition of an IO module in an IMU with a MicroLogic trip unit and an IFE communication interface.
-
The IMU has user-defined passwords for each user profile.
-
The IO module has the default passwords for each user profile.
Use EcoStruxure Power Commission software to replace the default passwords of the IO module by the user-defined passwords of the IMU for each user profile.
Password Reset
If the Administrator password of the (IMU) is lost or forgotten, the password can be reset to the default password with EcoStruxure Power Commission software and the support of the Schneider Electric Customer Care Center.
WARNING