Maintenance Indicators
Rate of Wear Counter
The contacts must be inspected each time the counter reaches a hundred mark. The message is displayed if the characteristics of the circuit breaker have not been defined. In this case, see in the menu on the MicroLogic HMI, in registers 9846–9853.
|
Address |
Register |
RW |
X |
Unit |
Type |
Range |
A/E/P/H |
Description |
|---|---|---|---|---|---|---|---|---|
|
0x2385 |
9094 |
R |
1 |
% |
INT16U |
0–32767 |
P/H |
Phase 1 contact wear indicator (1) |
|
0x2386 |
9095 |
R |
1 |
% |
INT16U |
0–32767 |
P/H |
Phase 2 contact wear indicator (1) |
|
0x2387 |
9096 |
R |
1 |
% |
INT16U |
0–32767 |
P/H |
Phase 3 contact wear indicator (1) |
|
0x2388 |
9097 |
R |
1 |
% |
INT16U |
0–32767 |
P/H |
Neutral contact wear indicator (1) |
|
(1) Factory setting = 0x8000. |
||||||||
Load Profile Counters
The load profile counters (only available with the BCM ULP module) report the number of hours for each range of current in the MicroLogic trip unit. If the load profile counters reach the maximum value 4 294 967 295 and a new load profile event occurs, then the load profile counters are reset to 0.
A read request of eight registers is necessary to read the load profile counters.
|
Address |
Register |
RW |
X |
Unit |
Type |
Range |
A/E/P/H |
Description |
|---|---|---|---|---|---|---|---|---|
|
0x74B7–0x74B8 |
29880–29881 |
R |
1 |
Hour |
INT32U |
0–4 294 967 295 |
A/E/P/H |
Number of hours for 0–49% of the nominal current range |
|
0x74B9–0x74BA |
29882–29883 |
R |
1 |
Hour |
INT32U |
0–4 294 967 295 |
A/E/P/H |
Number of hours for 50–79% of the nominal current range |
|
0x74BB–0x74BC |
29884–29885 |
R |
1 |
Hour |
INT32U |
0–4 294 967 295 |
A/E/P/H |
Number of hours for 80–89% of the nominal current range |
|
0x74BD–0x74BE |
29886–29887 |
R |
1 |
Hour |
INT32U |
0–4 294 967 295 |
A/E/P/H |
Number of hours for 90–100% of the nominal current range |