DOCA0384EN-01

Description of Commands with Session

Presentation

The procedure for setting a protection setting conforms to UL489SE standard. It is safeguarded by an exclusive editing session and by a two-step procedure for submitting and applying setting changes.

The exclusive editing session means that only one interface at a time can access and set protection settings. Access from other interfaces is blocked when an editing session is open.

During the editing session there is no impact on the active protection provided by the MicroLogic Active control unit until the new settings are applied. If the new settings are canceled, or the editing session times out before the new settings are applied, the active settings are maintained.

Enabling and Disabling Access to Protection Settings

You can enable or disable remote access to the protection settings on the MicroLogic Active display screen, from the tree navigation menu, at Configuration > Communication > Remote Settings.

  • Select ON to enable remote access to the protection settings

  • Select OFF to disable remote access to the protection settings

Editing Session for Selecting and Changing Protection Settings

An editing session has the following characteristics:

  • Only one editing session at a time can be open. Access to protection settings from other interfaces is blocked when you open an editing session.

  • There is a five-minute timeout for submitting and for applying new settings. The session times out as follows:

    • Five minutes after the session opens, if you do not submit the new settings

    • Five minutes after submitting the new settings, if you do not apply the new settings

  • After applying new settings, get the apply setting status to check that the new protection settings are applied. Once apply is completed, close the session.

  • When setting protection using the communication network, all protection functions can be set in one editing session. A submit step is required after making changes to each protection function, and one apply step is required to apply all the new settings. Active settings are maintained until the apply step is executed.

  • The neutral protection can be set with the standard protections.

Two-Step Procedure for Submitting and Applying Protection Settings

The procedure for changing protection settings requires you to submit and apply the new settings in two consecutive steps:

Step

Action

1

Submit new settings

Select new settings required and submit. The new settings are displayed so that you can check that the settings are correct before they are applied. Read the new settings to confirm that they are correct.

2

Apply new settings

Apply the new settings. The existing active protection settings are replaced by the new settings.

Protection Setting Procedure with Session

To set protection settings by using the communication network, external access to protection settings must be allowed by using the MicroLogic Active display screen.

The following example shows how to set the long-time overcurrent protection:

Step

Action

1

Open the editing session with the open setup session command .

Result: The session key for the editing session is returned to the command registers. The returned session key must be used in all commands during the session.

2

Submit the new protection settings with the submit long time over current protection settings command.

The requested session key for the command must be the session key returned by the open setup session command.

3

Use the get long time over current protection settings command to read the submitted settings.

The requested session key for the command must be the session key returned by the open setup session command.

4

Check that the protection settings submitted at step 2 and the protection settings got at step 3 are identical:

  • If the settings are identical, go to step 5

  • If the settings are not identical, go to step 7 and start the setting procedure again

5

Apply submitted protection settings with the apply settings command .

The requested session key for the command must be the session key returned by the open setup session command.

6

Use the get apply setting status to check that the new protection settings are applied.

The requested session key for the command must be the session key returned by the open setup session command.

NOTE: If the settings of other protection functions must be changed, restart the setting procedure at step 2 for each protection function.

7

Close the editing session with the close setup session command.

The requested session key for the command must be the session key returned by the open setup session command.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?