DOCA0384EN-01

Pre-Alarms

General Description

EcoStruxure Power Commission software enables the configuration of the following 3 pre-alarms:

  • Long-time protection pre-alarm (PAL Ir)

  • Ground-fault protection pre-alarm (PAL Ig)

  • Earth-leakage protection pre-alarm (PAL IΔn)

Each alarm has a corresponding alarm code:

  • PAL Ir = 1013

  • PAL Ig = 1014

  • PAL IΔn = 1015

Each alarm has a priority level that manages the alarm display on the FDM121 display:

  • No priority = N/A (not affected)

  • Low priority = 1. No alarm display on the FDM121 display.

  • Medium priority = 2. The FDM121 display LED is steady ON.

  • High priority = 3. The FDM121 display LED blinks and a pop-up screen informs the user that the alarm is active.

For more information regarding the relationship between alarm priority and FDM121 display, refer to the following guides in Related Documents at the beginning of this guide:

  • DOCA0188•• ComPacT NSX MicroLogic 5/6/7 Trip Units - User Guide

  • 48940-312-01 - MicroLogic 5 and 6 Electronic Trip Units for PowerPacT H-, J-, and L-Frame Circuit Breakers - User Guide

The pre-alarms registers describe the settings of the pre-alarms:

Address

Register

Description

0x19F9–0x1A02

6650–6659

Long-time protection pre-alarm (PAL Ir)

0x1A03–0x1A0C

6660–6669

Ground-fault protection pre-alarm (PAL Ig)

0x1A0D–0x1A16

6670–6679

Earth-leakage protection pre-alarm (PAL IΔn)

Long-Time Protection Pre-Alarm (PAL Ir)

A read request of 10 registers is necessary to read the long-time protection pre-alarm parameters.

Address

Register

RW

X

Unit

Type

Range

Description

0x19F9

6650

R

INT16U

The MSB gives the activity of the alarm: 0 = On, 1 = Off. The factory setting is 0 (On).

The LSB gives the priority of the alarm: N/A, 1, 2, or 3. The factory setting is 2 (medium priority).

0x19FA

6651

Reserved

0x19FB

6652

R

1

%

INT16

(1)

% of Ir pick-up value. The factory setting is 90.

0x19FC

6653

Reserved

0x19FD

6654

R

1

s

INT16U

1

Pick-up time delay (fixed to 1 s)

0x19FE

6655

R

1

%

INT16

(1)

% of Ir drop-out value. The factory setting is 85.

0x19FF

6656

Reserved

0x1A00

6657

R

1

s

INT16U

1

Drop-out time delay (fixed to 1 s)

0x1A01–0x1A02

6658– 6659

Reserved

(1) For distribution application, the range is 40–100. For motor application, the range is 10–95.

Ground-Fault Protection Pre-Alarm (PAL Ig)

A read request of 10 registers is necessary to read the ground-fault protection pre-alarm parameters.

Address

Register

RW

X

Unit

Type

Range

Description

0x1A03

6660

R

INT16U

The MSB gives the activity of the alarm: 0 = On, 1 = Off. The factory setting is 0 (On).

The LSB gives the priority of the alarm: N/A, 1, 2, or 3. The factory setting is 2 (medium priority).

0x1A04

6661

Reserved

0x1A05

6662

R

1

%

INT16

40–100

% of Ig pick-up value. The factory setting is 90.

0x1A06

6663

Reserved

0x1A07

6664

R

1

s

INT16U

1

Pick-up time delay (fixed to 1 s)

0x1A08

6665

R

1

%

INT16

40–100

% of Ig drop-out value. The factory setting is 85.

0x1A09

6666

Reserved

0x1A0A

6667

R

1

s

INT16U

1

Drop-out time delay (fixed to 1 s)

0x1A0B–0x1A0C

6668–6669

Reserved

Earth-Leakage Protection Pre-Alarm (PAL IΔn)

A read request of 10 registers is necessary to read the earth-leakage protection pre-alarm parameters.

Address

Register

RW

X

Unit

Type

Range

Description

0x1A0D

6670

R

INT16U

The MSB gives the activity of the alarm: 0 = On, 1 = Off. The factory setting is 0 (On).

The LSB gives the priority of the alarm: N/A, 1, 2, or 3. The factory setting is 2 (medium priority).

0x1A0E

6671

Reserved

0x1A0F

6672

R

1

%

INT16

50–80

% of IΔn pick-up value. The factory setting is 90.

0x1A10

6673

Reserved

0x1A11

6674

R

1

s

INT16U

1

Pick-up time delay (fixed to 1 s)

0x1A12

6675

R

1

%

INT16

50–80

% of IΔn drop-out value. The factory setting is 85.

0x1A13

6676

Reserved

0x1A14

6677

R

1

s

INT16U

1

Drop-out time delay (fixed to 1 s)

0x1A15– 0x1A16

6678– 6679

Reserved

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?