DOCA0384EN-01

Protection Settings

Active Neutral Protection Settings

Address

Register

RW

Unit

Type

Range

Description

0xAFC8

45001

R

INT16U

0–1

Neutral protection mode

  • 0 = Off

  • 1 = On (tripping)

0xAFC9

45002

R

INT16U

0–3

Neutral protection type

  • 0 = Off

  • 1 = Half neutral protection

  • 2 = Full neutral protection

  • 3 = Oversized neutral protection

Active Long Time Over Current Protection Settings

Address

Register

RW

Unit

Type

Range

Description

0xAFDE

45023

R

INT16U

0–1

Long time over current protection mode

  • 0 = Off

  • 1 = On (tripping)

0xAFDF

45024

R

INT16U

1

Long time over current protection curve

  • 1 = Inverse time (I2t = ON)

0xAFE0–0xAFE1

45025–45026

R

A

FLOAT32

Long time over current protection threshold

0xAFE2–0xAFE3

45027–45028

R

s

FLOAT32

Long time over current protection time delay

Active Short Time Over Current Protection Settings

Address

Register

RW

Unit

Type

Range

Description

0xAFE8

45033

R

INT16U

0–1

Short time over current protection mode

  • 0 = Off

  • 1 = On (tripping)

0xAFE9

45034

R

INT16U

0–1

Short time over current protection curve

  • 0 = Definite time (I2t = OFF)

  • 1 = Inverse time (I2t = ON)

0xAFEA–0xAFEB

45035–45036

R

FLOAT32

Short time over current protection threshold coefficient

0xAFEC–0xAFED

45037–45038

R

s

FLOAT32

Short time over current protection time delay

Active Instantaneous Protection Settings

Address

Register

RW

Unit

Type

Range

Description

0xAFF2

45043

R

INT16U

0–1

Instantaneous over current protection mode

  • 0 = Off

  • 1 = On (tripping)

0xAFF3

45044

R

INT16U

0–1

Instantaneous over current protection time delay mode:

  • 0 = Standard

  • 1 = Fast

0xAFF4–0xAFF5

45045–45046

R

FLOAT32

Instantaneous over current protection threshold coefficient

Active Ground Fault Protection Settings

Address

Register

RW

Unit

Type

Range

Description

0xAFFA

45051

R

INT16U

0–1

Ground fault protection mode

  • 0 = Off

  • 1 = On (tripping)

0xAFFB

45052

R

INT16U

0–1

Ground fault protection curve

  • 0 = Definite time (I2t = OFF)

  • 1 = Inverse time (I2t = ON)

0xAFFC–0xAFFD

45053–45054

R

A

FLOAT32

Ground fault protection threshold

0xAFFE–0xAFFF

45055–45056

R

s

FLOAT32

Ground fault protection time delay

Active Earth Leakage Protection Settings

Address

Register

RW

Unit

Type

Range

Description

0xB004

45061

R

INT16U

0–1

Earth leakage protection mode

  • 0 = Off

  • 1 = On

0xB005

45062

R

Reserved

0xB006–0xB007

45063–45064

R

A

FLOAT32

Earth leakage protection threshold

0xB008–0xB009

45065–45066

R

s

FLOAT32

0.06, 0.15, 0.23, 0.35, 0.80

Earth leakage protection time delay

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.