DOCA0384EN-01

Miscellaneous

Nominal Current

Address

Register

RW

X

Unit

Type

Range

A/E

Description

0x222D

8750

R

1

A

INT16U

0–8000

A/E

Rated circuit breaker current

Factory setting = 100 A (circuit breaker sensor plug not present)

TBC@PCA
Protection Setting Change Counter

Address

Register

RW

X

Unit

Type

Range

A/E

Description

0x2263

8804

R

INT16U

0–65535

E

TBC@PCA

Protection setting change counter, incremented each time a protection setting change is applied.

Battery Status

The following table represents the battery charge status:

Address

Register

RW

X

Unit

Type

Range

A/E

Description

0x228A

8843

R

1

%

INT16U

0–100

A/E

Battery-charge indicator:

100 % = U > 2800 mV

50 % = 2200 < U < 2800 mV

0 % = U < 2200 mV

Time Remaining Until Long-Time Tripping

Time remaining until long-time tripping is evaluated every second. If another protection is tripped, then time remaining until long-time tripping continues to be evaluated.

Address

Register

RW

X

Unit

Type

Range

A/E

Description

0x22A0–0x22A1

8865–8866

R

10

s

MOD 10000

E

Time remaining until long-time tripping

Language

This register indicates the language used by the control unit. It can be modified on the MicroLogic Active HMI.

Address

Register

RW

X

Unit

Type

Range

A/E

Bit

Description

0x258D

9614

R

INT16U

E

0

French

1

US English

2

UK English (factory setting)

3

German

4

Spanish

5

Italian

7

Chinese

8

Portugese

9

Optional language available on order from Schneider Electric

10–15

Reserved

Nominal Frequency

Address

Register

RW

X

Unit

Type

Range

A/E

Bit

Description

0x258E

9615

R

INT16U

E

0

50 / 60 Hz (factory setting)

1–15

Reserved

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.