DOCA0384EN-01

Real-Time Measurements

General Description

The real-time measurements are refreshed every second. Real-time measurements include:

  • Voltage and voltage unbalance

  • Current and current unbalance

  • Active, reactive, apparent, and distortion power

  • Reactive power with harmonic

  • Power factor and fundamental power factor

  • Frequency

  • THD (total harmonic distortion)

Voltage

Register = 0 if voltage < 25 V.

Address

Register

RW

X

Unit

Type

Range

Description

0x03E7

1000

R

1

V

INT16U

0–850

RMS phase-to-phase voltage V12

0x03E8

1001

R

1

V

INT16U

0–850

RMS phase-to-phase voltage V23

0x03E9

1002

R

1

V

INT16U

0–850

RMS phase-to-phase voltage V31

0x03EA

1003

R

1

V

INT16U

0–850

RMS phase-to-neutral voltage V1N (1)

0x03EB

1004

R

1

V

INT16U

0–850

RMS phase-to-neutral voltage V2N (1)

0x03EC

1005

R

1

V

INT16U

0–850

RMS phase-to-neutral voltage V3N (1)

0x03ED

1006

R

1

V

INT16U

0–850

Arithmetic mean of V12, V23, and V31: (V12 + V23 + V31) / 3 = Vavg L-L

0x03EE

1007

R

1

V

INT16U

0–850

Arithmetic mean of V1N, V2N, and V3N: (V1N + V2N + V3N) / 3 = Vavg L-N (1)

0x0478

1145

R

1

V

INT16U

0–850

Vmax: maximum of V12, V23, and V31 (2)

0x0479

1146

R

1

V

INT16U

0–850

Vmin: minimum of V12, V23, and V31 (2)

(1) This value is not available for motor application and not accessible when the system type in register 3314 is 30 or 31. Refer to System Type.

(2) This value can be reset with the reset minimum/maximum command. Refer to Reset Minimum/Maximum.

Voltage Unbalance

Address

Register

RW

X

Unit

Type

Range

Description

0x03EF

1008

R

10

%

INT16U

-1000–+1000

V12 phase-to-phase voltage unbalance in relation to the arithmetic mean of phase-to-phase voltages

0x03F0

1009

R

10

%

INT16U

-1000–+1000

V23 phase-to-phase voltage unbalance in relation to the arithmetic mean of phase-to-phase voltages

0x03F1

1010

R

10

%

INT16U

-1000–+1000

V31 phase-to-phase voltage unbalance in relation to the arithmetic mean of phase-to-phase voltages

0x03F2

1011

R

10

%

INT16U

-1000–+1000

V1N phase-to-neutral voltage unbalance in relation to the arithmetic mean of phase-to-neutral voltages (1)

0x03F3

1012

R

10

%

INT16U

-1000–+1000

V2N phase-to-neutral voltage unbalance in relation to the arithmetic mean of phase-to-neutral voltages (1)

0x03F4

1013

R

10

%

INT16U

-1000–+1000

V3N phase-to-neutral voltage unbalance in relation to the arithmetic mean of phase-to-neutral voltages (1)

0x03F5

1014

R

10

%

INT16U

-1000–+1000

Maximum phase-to-phase voltage unbalance value of registers 1008, 1009, and 1010 (2)

0x03F6

1015

R

10

%

INT16U

-1000–+1000

Maximum phase-to-neutral voltage unbalance value of registers 1011, 1012, and 1013 (1)(2)

(1) This value is not available for motor application and when the system type in register 3314 is 30 or 31. Refer to System Type.

(2) This value can be reset with the reset minimum/maximum command. Refer to Reset Minimum/Maximum.

Current

Address

Register

RW

X

Unit

Type

Range

Description

0x03F7

1016

R

1

A

INT16U

0–20xIn

RMS current on phase 1: I1

0x03F8

1017

R

1

A

INT16U

0–20xIn

RMS current on phase 2: I2

0x03F9

1018

R

1

A

INT16U

0–20xIn

RMS current on phase 3: I3

0x03FA

1019

R

1

A

INT16U

0–20xIn

RMS current on the neutral: IN (1)

0x03FB

1020

R

1

A

INT16U

0–20xIn

Maximum of I1, I2, I3, and IN (2)

0x03FC

1021

R

1

%Ig

INT16U

0–20xIn

Ground-fault current

0x03FD

1022

R

1

mA

INT16U

0–20xIn

Earth-leakage current

0x0401

1026

R

1

A

INT16U

0–20xIn

Minimum of I1, I2, and I3 (2)

0x0402

1027

R

1

A

INT16U

0–20xIn

Arithmetic mean of I1, I2, and I3: (I1 + I2 + I3) / 3 = Iavg

(1) This value is not available for motor application and when the system type in register 3314 is 31 or 40. Refer to System Type.

(2) This value can be reset with the reset minimum/maximum command. Refer to Reset Minimum/Maximum.

Current Unbalance

Address

Register

RW

X

Unit

Type

Range

Description

0x0403

1028

R

10

%

INT16

-1000–+1000

I1 current unbalance in relation to the arithmetic mean of the phase currents

0x0404

1029

R

10

%

INT16

-1000–+1000

I2 current unbalance in relation to the arithmetic mean of the phase currents

0x0405

1030

R

10

%

INT16

-1000–+1000

I3 current unbalance in relation to the arithmetic mean of the phase currents

0x0406

1031

R

10

%

INT16

-1000–+1000

IN current unbalance in relation to the arithmetic mean of the phase current (1)

0x0407

1032

R

10

%

INT16

-1000–+1000

Maximum current unbalance of registers 1028, 1029, and 1030 (2)

(1) This value is not available for motor application and when the system type in register 3314 is 31 or 40. Refer to System Type.

(2) This value can be reset with the reset minimum/maximum command. Refer to Reset Minimum/Maximum.

Active Power

The flow sign of the active power depends on the configuration of register 3316. Refer to Power Flow Sign.

Address

Register

RW

X

Unit

Type

Range

Description

0x0409

1034

R

10

kW

INT16

-10000–+10000

Active power on phase 1: P1 (1)

0x040A

1035

R

10

kW

INT16

-10000–+10000

Active power on phase 2: P2 (1)

0x040B

1036

R

10

kW

INT16

-10000–+10000

Active power on phase 3: P3 (1)

0x040C

1037

R

10

kW

INT16

-30000–+30000

Total active power: Ptot

(1) This value is not available for motor application and when the system type in register 3314 is 30 or 31. Refer to System Type.

Reactive Power

The flow sign of the reactive power depends on the configuration of register 3316 Power Flow Sign.

Address

Register

RW

X

Unit

Type

Range

Description

0x040D

1038

R

10

kvar

INT16

-10000–+10000

Reactive power on phase 1: Q1 (1)

0x040E

1039

R

10

kvar

INT16

-10000–+10000

Reactive power on phase 2: Q2 (1)

0x040F

1040

R

10

kvar

INT16

-10000–+10000

Reactive power on phase 3: Q3 (1)

0x0410

1041

R

10

kvar

INT16

-30000–+30000

Total reactive power: Qtot

(1) This value is not available for motor application and when the system type in register 3314 is 30 or 31. Refer to System Type.

Apparent Power

Address

Register

RW

X

Unit

Type

Range

Description

0x0411

1042

R

10

kVA

INT16

0–10000

Apparent power on phase 1: S1 (1)

0x0412

1043

R

10

kVA

INT16

0–10000

Apparent power on phase 2: S2 (1)

0x0413

1044

R

10

kVA

INT16

0–10000

Apparent power on phase 3: S3 (1)

0x0414

1045

R

10

kVA

INT16

0–30000

Total apparent power: Stot

(1) This value is not available for motor application and when the system type in register 3314 is 30 or 31. Refer to System Type.

Power Factor

The sign of the power factor depends on the configuration of register 3318 Power Factor Sign.

Address

Register

RW

X

Unit

Type

Range

Description

0x0415

1046

R

100

INT16

-100–+100

Power factor on phase 1: PF1 (1)

0x0416

1047

R

100

INT16

-100–+100

Power factor on phase 2: PF2 (1)

0x0417

1048

R

100

INT16

-100–+100

Power factor on phase 3: PF3 (1)

0x0418

1049

R

100

INT16

-100–+100

Total power factor: PF

(1) This value is not available for motor application and when the system type in register 3314 is 30 or 31. Refer to System Type.

Fundamental Power Factor (cosϕ)

The sign of the fundamental power factor (cosϕ) depends on the configuration of register 3318 Power Factor Sign.

Address

Register

RW

X

Unit

Type

Range

Description

0x0419

1050

R

100

INT16

-100–+100

Fundamental power factor on phase 1: cosϕ 1 (1)

0x041A

1051

R

100

INT16

-100–+100

Fundamental power factor on phase 2: cosϕ 2 (1)

0x041B

1052

R

100

INT16

-100–+100

Fundamental power factor on phase 3: cosϕ 3 (1)

0x041C

1053

R

100

INT16

-100–+100

Total fundamental power factor: cosφ

(1) This value is not available for motor application and when the system type in register 3314 is 30 or 31. Refer to System Type.

Frequency

When the MicroLogic 5/6/7 trip unit cannot calculate the frequency, it returns Not Evaluated = 32768 (0x8000).

Address

Register

RW

X

Unit

Type

Range

Description

0x041D

1054

R

10

Hz

INT16U

150–4400

System frequency: F

Fundamental Reactive Power

The flow sign of the reactive power depends on the configuration of register 3316 Power Flow Sign.

Address

Register

RW

X

Unit

Type

Range

Description

0x0437

1080

R

10

kvar

INT16

-10000–+10000

Fundamental reactive power on phase 1: Q1 Fund (1)

0x0438

1081

R

10

kvar

INT16

-10000–+10000

Fundamental reactive power on phase 2: Q2 Fund (1)

0x0439

1082

R

10

kvar

INT16

-10000–+10000

Fundamental reactive power on phase 3: Q3 Fund (1)

0x043A

1083

R

10

kvar

INT16

-10000–+10000

Total fundamental reactive power: Qtot Fund

(1) This value is not available for motor application and when the system type in register 3314 is 30 or 31. Refer to System Type.

Distortion Power

Address

Register

RW

X

Unit

Type

Range

Description

0x043F

1088

R

10

kvar

INT16U

0–10000

Distortion power on phase 1: D1 (1)

0x0440

1089

R

10

kvar

INT16U

0–10000

Distortion power on phase 2: D2 (1)

0x0441

1090

R

10

kvar

INT16U

0–10000

Distortion power on phase 3: D3 (1)

0x0442

1091

R

10

kvar

INT16U

0–10000

Total distortion power: Dtot

(1) This value is not available for motor application and when the system type in register 3314 is 30 or 31. Refer to System Type.

Total Harmonic Distortion (THD)

Address

Register

RW

X

Unit

Type

Range

Description

0x0443

1092

R

10

%

INT16U

0–32766

Total harmonic distortion of V12 in relation to the fundamental

0x0444

1093

R

10

%

INT16U

0–32766

Total harmonic distortion of V23 in relation to the fundamental

0x0445

1094

R

10

%

INT16U

0–32766

Total harmonic distortion of V31 in relation to the fundamental

0x0446

1095

R

10

%

INT16U

0–32766

Total harmonic distortion of V1N in relation to the fundamental (1)

0x0447

1096

R

10

%

INT16U

0–32766

Total harmonic distortion of V2N in relation to the fundamental (1)

0x0448

1097

R

10

%

INT16U

0–32766

Total harmonic distortion of V3N in relation to the fundamental (1)

0x0449

1098

R

10

%

INT16U

0–32766

Total harmonic distortion of I1 in relation to the fundamental

0x044A

1099

R

10

%

INT16U

0–32766

Total harmonic distortion of I2 in relation to the fundamental

0x044B

1100

R

10

%

INT16U

0–32766

Total harmonic distortion of I3 in relation to the fundamental

(1) This value is not available for motor application and when the system type in register 3314 is 30 or 31. Refer to System Type.

Thermal Image of Motor

Address

Register

RW

X

Unit

Type

Range

Description

0x0477

1144

R

1

%

INT16U

0–32766

Ith image

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?