DOCA0384EN-01

Energy Measurements

Active, Reactive, and Apparent Energy

Address

Register

RW

Unit

Type

Range

Description

0x7D5F–0x7D62

32096–32099

R

Wh

INT64

Total active energy(1)

0x7D63–0x7D66

32100–32103

R

VARh

INT64

Total reactive energy(1)

0x7D67–0x7D6A

32104–32107

R

Wh

INT64U

Total active energy delivered (into the load, counted positively)(1)

0x7D6B–0x7D6E

32108–32111

R

Wh

INT64U

Total active energy received (out of the load, counted negatively)(1)

0x7D6F–0x7D72

32112–32115

R

VARh

INT64U

Total reactive energy delivered (into the load, counted positively) (1)

0x7D73–0x7D76

32116–32119

R

VARh

INT64U

Total reactive energy received (out of the load, counted negatively)(1)

0x7D77–0x7D7A

32120–32123

R

VAh

INT64U

Total apparent energy(1)

0x7D7B–0x7D7E

32124–32127

R

Wh

INT64U

Total cumulative active energy delivered (into the load, counted positively, not resettable)

0x7D7F–0x7D82

32128–32131

R

Wh

INT64U

Total cumulative active energy received (out of the load, counted negatively, not resettable)

(1) Value reset with the reset energies command.

Address

Register

RW

Unit

Type

Range

Description

0x5608–0x560B

22025–22028

R

Wh

INT64

Total cumulative active energy (not resettable)

0x560C–0x5617

22029–22040

Reserved

0x5618–0x561B

22041–22044

R

VArh

INT64

Total cumulative reactive energy (not resettable)

0x561C–0x561F

22045-22048

R

VArh

INT64

Total cumulative reactive energy delivered (out of the load, counted positively, not resettable)

0x5620–0x5623

22049–22052

R

VArh

INT64

Total cumulative reactive energy received (into the load, counted negatively, not resettable)

0x5624–0x5627

22053–22056

R

VAh

INT64

Total cumulative apparent energy (not resettable)

Timestamp of Reset Actions

Address

Register

RW

Unit

Type

Range

Description

0x8968–0x896B

35177–35180

R

DATETIME

Timestamp of last reset of accumulated energy

Energy per Phase

Energy per phase is available when the Energy per Phase Digital Module is purchased and installed on a MicroLogic X control unit.

Address

Register

RW

Unit

Type

Range

Description

0xAD70–0xAD73

44401–44404

R

Wh

INT64

Active energy delivered on phase 1 (into the load, counted positively)(1)

0xAD74–0xAD77

44405–44408

R

Wh

INT64

Active energy received on phase 1 (out of the load, counted negatively)(1)

0xAD78–0xAD7B

44409–44412

R

Wh

INT64

Total active energy delivered on phase 1 (not resettable)

0xAD7C–0xAD7F

44413–44416

R

Wh

INT64

Total active energy received on phase 1 (not resettable)

0xAD80–0xAD83

44417–44420

R

Wh

INT64

Active energy delivered on phase 2 (into the load, counted positively)(1)

0xAD84–0xAD87

44421–44424

R

Wh

INT64

Active energy received on phase 2 (out of the load, counted negatively)(1)

0xAD88–0xAD8B

44425–44428

R

Wh

INT64

Total active energy delivered on phase 2 (not resettable)

0xAD8C–0xAD8F

44429–44432

R

Wh

INT64

Total active energy received on phase 2 (not resettable)

0xAD90–0xAD93

44433–44436

R

Wh

INT64

Active energy delivered on phase 3 (into the load, counted positively)(1)

0xAD94–0xAD97

44437–44440

R

Wh

INT64

Active energy received on phase 3 (out of the load, counted negatively)(1)

0xAD98–0xAD9B

44441–44444

R

Wh

INT64

Total active energy delivered on phase 3 (not resettable)

0xAD9C–0xAD9F

44445–44448

R

Wh

INT64

Total active energy received on phase 3 (not resettable)

0xADA0–0xADA3

44449–44452

R

VArh

INT64

Reactive energy delivered on phase 1 (into the load, counted positively)(1)

0xADA4–0xADA7

44453–44456

R

VArh

INT64

Reactive energy received on phase 1 (out of the load, counted negatively)(1)

0xADA8–0xADAB

44457–44460

R

VArh

INT64

Total reactive energy delivered on phase 1 (not resettable)

0xADAC–0xADAF

44461–44464

R

VArh

INT64

Total reactive energy received on phase 1(not resettable)

0xADB0–0xADB3

44465–44468

R

VArh

INT64

Reactive energy delivered on phase 2 (into the load, counted positively)(1)

0xADB4–0xADB7

44469–44472

R

VArh

INT64

Reactive energy received on phase 2 (out of the load, counted negatively)(1)

0xADB8–0xADBB

44473–44476

R

VArh

INT64

Total reactive energy delivered on phase 2 (not resettable)

0xADBC–0xADBF

44477–44480

R

VArh

INT64

Total reactive energy received on phase 2 (not resettable)

0xADC0–0xADC3

44481–44484

R

VArh

INT64

Reactive energy delivered on phase 3 (into the load, counted positively)(1)

0xADC4–0xADC7

44485–44488

R

VArh

INT64

Reactive energy received on phase 3 (out of the load, counted negatively)(1)

0xADC8–0xADCB

44489–44492

R

VArh

INT64

Total reactive energy delivered on phase 3 (not resettable)

0xADCC–0xADCF

44493–44496

R

VArh

INT64

Total reactive energy received on phase 3 (not resettable)

0xADD0–0xADD3

44497–44500

R

VAh

INT64

Apparent energy on phase 1(1)

0xADD4–0xADD7

44501–44504

R

VAh

INT64

Cumulative apparent energy on phase 1 (not resettable)

0xADD8–0xADDB

44505–44508

R

VAh

INT64

Apparent energy on phase 2(1)

0xADDC–0xADDF

44509–44512

R

VAh

INT64

Cumulative apparent energy on phase 2 (not resettable)

0xADE0–0xADE3

44513–44516

R

VAh

INT64

Apparent energy on phase 3(1)

0xADE4–0xADE7

44517–44520

R

VAh

INT64

Cumulative apparent energy on phase 3 (not resettable)

(1) Value reset with the reset energies command.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?