DOCA0384EN-01

Spectral Components

Overview

Parity

Spectral Component

Addresses

Registers

Odd rank

Amplitude of voltage harmonic

0x1003–0x105C

4100–4189

Amplitude of current harmonic

0x105D–0x1098

4190–4249

Phase of voltage harmonic

0x1099–0x10AA

4250–4267

Phase of current harmonic

0x10F3–0x1102

4340–4355

Even rank

Amplitude of voltage harmonic

0x112F–0x1188

4400–4489

Amplitude of current harmonic

0x1189–0x11C4

4490–4549

Phase of voltage harmonic

0x11C5–0x11D6

4550–4567

Phase of current harmonic

0x121F–0x122E

4640–4655

Only the registers of the odd rank harmonics are detailed:

  • The registers of the even rank harmonics (n) are equal to the registers of the odd rank harmonics (n+1) plus 300.

  • The order of the even rank registers is the same as that of the odd rank registers.

  • The scale factor of the even rank registers is the same as that of the odd rank registers.

Amplitude of Odd Rank Voltage Harmonic

The amplitude of odd rank voltage harmonic is expressed as a ratio in % to the amplitude of the fundamental (not applicable in 400 Hz nominal frequency system):

Address

Register

RW

X

Unit

Type

Range

A/E/P/H

Description

0x1003

4100

R

10

%

INT16U

0–1200

H

Harmonic 3 of V12

0x1004

4101

R

10

%

INT16U

0–1200

H

Harmonic 3 of V23

0x1005

4102

R

10

%

INT16U

0–1200

H

Harmonic 3 of V31

0x1006

4103

R

10

%

INT16U

0–1200

H

Harmonic 3 of V1N (1)

0x1007

4104

R

10

%

INT16U

0–1200

H

Harmonic 3 of V2N (1)

0x1008

4105

R

10

%

INT16U

0–1200

H

Harmonic 3 of V3N (1)

0x1009

4106

R

10

%

INT16U

0–1200

H

Harmonic 5 of V12

0x100A

4107

R

10

%

INT16U

0–1200

H

Harmonic 5 of V23

0x100B

4108

R

10

%

INT16U

0–1200

H

Harmonic 5 of V31

0x100C

4109

R

10

%

INT16U

0–1200

H

Harmonic 5 of V1N (1)

0x100D

4110

R

10

%

INT16U

0–1200

H

Harmonic 5 of V2N (1)

0x100E

4111

R

10

%

INT16U

0–1200

H

Harmonic 5 of V3N

0x100F

4112

R

10

%

INT16U

0–1200

H

Harmonic 7 of V12

0x1010

4113

R

10

%

INT16U

0–1200

H

Harmonic 7 of V23

0x1011

4114

R

10

%

INT16U

0–1200

H

Harmonic 7 of V31

0x1012

4115

R

10

%

INT16U

0–1200

H

Harmonic 7 of V1N (1)

0x1013

4116

R

10

%

INT16U

0–1200

H

Harmonic 7 of V2N (1)

0x1014

4117

R

10

%

INT16U

0–1200

H

Harmonic 7 of V3N (1)

0x1015

4118

R

10

%

INT16U

0–1200

H

Harmonic 9 of V12

0x1016

4119

R

10

%

INT16U

0–1200

H

Harmonic 9 of V23

0x1017

4120

R

10

%

INT16U

0–1200

H

Harmonic 9 of V31

0x1018

4121

R

10

%

INT16U

0–1200

H

Harmonic 9 of V1N (1)

0x1019

4122

R

10

%

INT16U

0–1200

H

Harmonic 9 of V2N (1)

0x101A

4123

R

10

%

INT16U

0–1200

H

Harmonic 9 of V3N (1)

0x101B

4124

R

10

%

INT16U

0–1200

H

Harmonic 11 of V12

0x101C

4125

R

10

%

INT16U

0–1200

H

Harmonic 11 of V23

0x101D

4126

R

10

%

INT16U

0–1200

H

Harmonic 11 of V31

0x101E

4127

R

10

%

INT16U

0–1200

H

Harmonic 11 of V1N (1)

0x101F

4128

R

10

%

INT16U

0–1200

H

Harmonic 11 of V2N (1)

0x1020

4129

R

10

%

INT16U

0–1200

H

Harmonic 11 of V3N (1)

0x1021

4130

R

10

%

INT16U

0–1200

H

Harmonic 13 of V12

0x1022

4131

R

10

%

INT16U

0–1200

H

Harmonic 13 of V23

0x1023

4132

R

10

%

INT16U

0–1200

H

Harmonic 13 of V31

0x1024

4133

R

10

%

INT16U

0–1200

H

Harmonic 13 of V1N (1)

0x1025

4134

R

10

%

INT16U

0–1200

H

Harmonic 13 of V2N (1)

0x1026

4135

R

10

%

INT16U

0–1200

H

Harmonic 13 of V3N (1)

0x1027

4136

R

10

%

INT16U

0–1200

H

Harmonic 15 of V12

0x1028

4137

R

10

%

INT16U

0–1200

H

Harmonic 15 of V23

0x1029

4138

R

10

%

INT16U

0–1200

H

Harmonic 15 of V31

0x102A

4139

R

10

%

INT16U

0–1200

H

Harmonic 15 of V1N (1)

0x102B

4140

R

10

%

INT16U

0–1200

H

Harmonic 15 of V2N (1)

0x102C

4141

R

10

%

INT16U

0–1200

H

Harmonic 15 of V3N (1)

0x102D

4142

R

10

%

INT16U

0–1200

H

Harmonic 17 of V12

0x102E

4143

R

10

%

INT16U

0–1200

H

Harmonic 17 of V23

0x102F

4144

R

10

%

INT16U

0–1200

H

Harmonic 17 of V31

0x1030

4145

R

10

%

INT16U

0–1200

H

Harmonic 17 of V1N (1)

0x1031

4146

R

10

%

INT16U

0–1200

H

Harmonic 17 of V2N (1)

0x1032

4147

R

10

%

INT16U

0–1200

H

Harmonic 17 of V3N (1)

0x1033

4148

R

10

%

INT16U

0–1200

H

Harmonic 19 of V12

0x1034

4149

R

10

%

INT16U

0–1200

H

Harmonic 19 of V23

0x1035

4150

R

10

%

INT16U

0–1200

H

Harmonic 19 of V31

0x1036

4151

R

10

%

INT16U

0–1200

H

Harmonic 19 of V1N (1)

0x1037

4152

R

10

%

INT16U

0–1200

H

Harmonic 19 of V2N (1)

0x1038

4153

R

10

%

INT16U

0–1200

H

Harmonic 19 of V3N (1)

0x1039

4154

R

10

%

INT16U

0–1200

H

Harmonic 21 of V12

0x103A

4155

R

10

%

INT16U

0–1200

H

Harmonic 21 of V23

0x103B

4156

R

10

%

INT16U

0–1200

H

Harmonic 21 of V31

0x103C

4157

R

10

%

INT16U

0–1200

H

Harmonic 21 of V1N (1)

0x103D

4158

R

10

%

INT16U

0–1200

H

Harmonic 21 of V2N (1)

0x103E

4159

R

10

%

INT16U

0–1200

H

Harmonic 21 of V3N (1)

0x103F

4160

R

10

%

INT16U

0–1200

H

Harmonic 23 of V12

0x1040

4161

R

10

%

INT16U

0–1200

H

Harmonic 23 of V23

0x1041

4162

R

10

%

INT16U

0–1200

H

Harmonic 23 of V31

0x1042

4163

R

10

%

INT16U

0–1200

H

Harmonic 23 of V1N (1)

0x1043

4164

R

10

%

INT16U

0–1200

H

Harmonic 23 of V2N (1)

0x1044

4165

R

10

%

INT16U

0–1200

H

Harmonic 23 of V3N (1)

0x1045

4166

R

10

%

INT16U

0–1200

H

Harmonic 25 of V12

0x1046

4167

R

10

%

INT16U

0–1200

H

Harmonic 25 of V23

0x1047

4168

R

10

%

INT16U

0–1200

H

Harmonic 25 of V31

0x1048

4169

R

10

%

INT16U

0–1200

H

Harmonic 25 of V1N (1)

0x1049

4170

R

10

%

INT16U

0–1200

H

Harmonic 25 of V2N (1)

0x104A

4171

R

10

%

INT16U

0–1200

H

Harmonic 25 of V3N (1)

0x104B

4172

R

10

%

INT16U

0–1200

H

Harmonic 27 of V12

0x104C

4173

R

10

%

INT16U

0–1200

H

Harmonic 27 of V23

0x104D

4174

R

10

%

INT16U

0–1200

H

Harmonic 27 of V31

0x104E

4175

R

10

%

INT16U

0–1200

H

Harmonic 27 of V1N (1)

0x104F

4176

R

10

%

INT16U

0–1200

H

Harmonic 27 of V2N (1)

0x1050

4177

R

10

%

INT16U

0–1200

H

Harmonic 27 of V3N (1)

0x1051

4178

R

10

%

INT16U

0–1200

H

Harmonic 29 of V12

0x1052

4179

R

10

%

INT16U

0–1200

H

Harmonic 29 of V23

0x1053

4180

R

10

%

INT16U

0–1200

H

Harmonic 29 of V31

0x1054

4181

R

10

%

INT16U

0–1200

H

Harmonic 29 of V1N (1)

0x1055

4182

R

10

%

INT16U

0–1200

H

Harmonic 29 of V2N (1)

0x1056

4183

R

10

%

INT16U

0–1200

H

Harmonic 29 of V3N (1)

0x1057

4184

R

10

%

INT16U

0–1200

H

Harmonic 31 of V12

0x1058

4185

R

10

%

INT16U

0–1200

H

Harmonic 31 of V23

0x1059

4186

R

10

%

INT16U

0–1200

H

Harmonic 31 of V31

0x105A

4187

R

10

%

INT16U

0–1200

H

Harmonic 31 of V1N (1)

0x105B

4188

R

10

%

INT16U

0–1200

H

Harmonic 31 of V2N (1)

0x105C

4189

R

10

%

INT16U

0–1200

H

Harmonic 31 of V3N (1)

(1) Value is not available when the system type in register 3314 is 31. Refer to System Type.

Amplitude of Odd Rank Current Harmonic

The amplitude of odd rank current harmonic is expressed as a ratio in % to the amplitude of the fundamental (not applicable in 400 Hz nominal frequency system):

Address

Register

RW

X

Unit

Type

Range

A/E/P/H

Description

0x105D

4190

R

10

%

INT16U

0–32767

H

Harmonic 3 of I1

0x105E

4191

R

10

%

INT16U

0–32767

H

Harmonic 3 of I2

0x105F

4192

R

10

%

INT16U

0–32767

H

Harmonic 3 of I3

0x1060

4193

R

10

%

INT16U

0–32767

H

Harmonic 3 of IN (1)

0x1061

4194

R

10

%

INT16U

0–32767

H

Harmonic 5 of I1

0x1062

4195

R

10

%

INT16U

0–32767

H

Harmonic 5 of I2

0x1063

4196

R

10

%

INT16U

0–32767

H

Harmonic 5 of I3

0x1064

4197

R

10

%

INT16U

0–32767

H

Harmonic 5 of IN (1)

0x1065

4198

R

10

%

INT16U

0–32767

H

Harmonic 7 of I1

0x1066

4199

R

10

%

INT16U

0–32767

H

Harmonic 7 of I2

0x1067

4200

R

10

%

INT16U

0–32767

H

Harmonic 7 of I3

0x1068

4201

R

10

%

INT16U

0–32767

H

Harmonic 7 of IN (1)

0x1069

4202

R

10

%

INT16U

0–32767

H

Harmonic 9 of I1

0x106A

4203

R

10

%

INT16U

0–32767

H

Harmonic 9 of I2

0x106B

4204

R

10

%

INT16U

0–32767

H

Harmonic 9 of I3

0x106C

4205

R

10

%

INT16U

0–32767

H

Harmonic 9 of IN (1)

0x106D

4206

R

10

%

INT16U

0–32767

H

Harmonic 11 of I1

0x106E

4207

R

10

%

INT16U

0–32767

H

Harmonic 11 of I2

0x106F

4208

R

10

%

INT16U

0–32767

H

Harmonic 11 of I3

0x1070

4209

R

10

%

INT16U

0–32767

H

Harmonic 11 of IN (1)

0x1071

4210

R

10

%

INT16U

0–32767

H

Harmonic 13 of I1

0x1072

4211

R

10

%

INT16U

0–32767

H

Harmonic 13 of I2

0x1073

4212

R

10

%

INT16U

0–32767

H

Harmonic 13 of I3

0x1074

4213

R

10

%

INT16U

0–32767

H

Harmonic 13 of IN (1)

0x1075

4214

R

10

%

INT16U

0–32767

H

Harmonic 15 of I1

0x1076

4215

R

10

%

INT16U

0–32767

H

Harmonic 15 of I2

0x1077

4216

R

10

%

INT16U

0–32767

H

Harmonic 15 of I3

0x1078

4217

R

10

%

INT16U

0–32767

H

Harmonic 15 of IN (1)

0x1079

4218

R

10

%

INT16U

0–32767

H

Harmonic 17 of I1

0x107A

4219

R

10

%

INT16U

0–32767

H

Harmonic 17 of I2

0x107B

4220

R

10

%

INT16U

0–32767

H

Harmonic 17 of I3

0x107C

4221

R

10

%

INT16U

0–32767

H

Harmonic 17 of IN (1)

0x107D

4222

R

10

%

INT16U

0–32767

H

Harmonic 19 of I1

0x107E

4223

R

10

%

INT16U

0–32767

H

Harmonic 19 of I2

0x107F

4224

R

10

%

INT16U

0–32767

H

Harmonic 19 of I3

0x1080

4225

R

10

%

INT16U

0–32767

H

Harmonic 19 of IN (1)

0x1081

4226

R

10

%

INT16U

0–32767

H

Harmonic 21 of I1

0x1082

4227

R

10

%

INT16U

0–32767

H

Harmonic 21 of I2

0x1083

4228

R

10

%

INT16U

0–32767

H

Harmonic 21 of I3

0x1084

4229

R

10

%

INT16U

0–32767

H

Harmonic 21 of IN (1)

0x1085

4230

R

10

%

INT16U

0–32767

H

Harmonic 23 of I1

0x1086

4231

R

10

%

INT16U

0–32767

H

Harmonic 23 of I2

0x1087

4232

R

10

%

INT16U

0–32767

H

Harmonic 23 of I3

0x1088

4233

R

10

%

INT16U

0–32767

H

Harmonic 23 of IN (1)

0x1089

4234

R

10

%

INT16U

0–32767

H

Harmonic 25 of I1

0x108A

4235

R

10

%

INT16U

0–32767

H

Harmonic 25 of I2

0x108B

4236

R

10

%

INT16U

0–32767

H

Harmonic 25 of I3

0x108C

4237

R

10

%

INT16U

0–32767

H

Harmonic 25 of IN (1)

0x108D

4238

R

10

%

INT16U

0–32767

H

Harmonic 27 of I1

0x108E

4239

R

10

%

INT16U

0–32767

H

Harmonic 27 of I2

0x108F

4240

R

10

%

INT16U

0–32767

H

Harmonic 27 of I3

0x1090

4241

R

10

%

INT16U

0–32767

H

Harmonic 27 of IN (1)

0x1091

4242

R

10

%

INT16U

0–32767

H

Harmonic 29 of I1

0x1092

4243

R

10

%

INT16U

0–32767

H

Harmonic 29 of I2

0x1093

4244

R

10

%

INT16U

0–32767

H

Harmonic 29 of I3

0x1094

4245

R

10

%

INT16U

0–32767

H

Harmonic 29 of IN (1)

0x1095

4246

R

10

%

INT16U

0–32767

H

Harmonic 31 of I1

0x1096

4247

R

10

%

INT16U

0–32767

H

Harmonic 31 of I2

0x1097

4248

R

10

%

INT16U

0–32767

H

Harmonic 31 of I3

0x1098

4249

R

10

%

INT16U

0–32767

H

Harmonic 31 of IN (1)

(1) Value is not available when the system type in register 3314 is 31. Refer to System Type.

Phase of Odd Rank Voltage Harmonic

These registers contain the odd rank voltage harmonic phase value (not applicable in 400 Hz nominal frequency system):

Address

Register

RW

X

Unit

Type

Range

A/E/P/H

Description

0x1099

4250

R

10

Deg

INT16U

0–3600

H

Phase of harmonic 3 of V12

0x109A

4251

R

10

Deg

INT16U

0–3600

H

Phase of harmonic 3 of V23

0x109B

4252

R

10

Deg

INT16U

0–3600

H

Phase of harmonic 3 of V31

0x109C

4253

R

10

Deg

INT16U

0–3600

H

Phase of harmonic 3 of V1N (1)

0x109D

4254

R

10

Deg

INT16U

0–3600

H

Phase of harmonic 3 of V2N (1)

0x109E

4255

R

10

Deg

INT16U

0–3600

H

Phase of harmonic 3 of V3N (1)

0x109F

4256

R

10

Deg

INT16U

0–3600

H

Phase of harmonic 5 of V12

0x10A0

4257

R

10

Deg

INT16U

0–3600

H

Phase of harmonic 5 of V23

0x10A1

4258

R

10

Deg

INT16U

0–3600

H

Phase of harmonic 5 of V31

0x10A2

4259

R

10

Deg

INT16U

0–3600

H

Phase of harmonic 5 of V1N (1)

0x10A3

4260

R

10

Deg

INT16U

0–3600

H

Phase of harmonic 5 of V2N (1)

0x10A4

4261

R

10

Deg

INT16U

0–3600

H

Phase of harmonic 5 of V3N (1)

0x10A5

4262

R

10

Deg

INT16U

0–3600

H

Phase of harmonic 7 of V12

0x10A6

4263

R

10

Deg

INT16U

0–3600

H

Phase of harmonic 7 of V23

0x10A7

4264

R

10

Deg

INT16U

0–3600

H

Phase of harmonic 7 of V31

0x10A8

4265

R

10

Deg

INT16U

0–3600

H

Phase of harmonic 7 of V1N (1)

0x10A9

4266

R

10

Deg

INT16U

0–3600

H

Phase of harmonic 7 of V2N (1)

0x10AA

4267

R

10

Deg

INT16U

0–3600

H

Phase of harmonic 7 of V3N (1)

(1) Value is not available when the system type in register 3314 is 31. Refer to System Type.

Phase of Odd Rank Current Harmonic

These registers contain the odd rank current harmonic phase value (not applicable in 400 Hz nominal frequency system):

Address

Register

RW

X

Unit

Type

Range

A/E/P/H

Description

0x10F3

4340

R

10

Deg

INT16U

0–3600

H

Phase of harmonic 3 of I1

0x10F4

4341

R

10

Deg

INT16U

0–3600

H

Phase of harmonic 3 of I2

0x10F5

4342

R

10

Deg

INT16U

0–3600

H

Phase of harmonic 3 of I3

0x10F6

4343

R

10

Deg

INT16U

0–3600

H

Phase of harmonic 3 of IN (1)

0x10F7

4344

R

10

Deg

INT16U

0–3600

H

Phase of harmonic 5 of I1

0x10F8

4345

R

10

Deg

INT16U

0–3600

H

Phase of harmonic 5 of I2

0x10F9

4346

R

10

Deg

INT16U

0–3600

H

Phase of harmonic 5 of I3

0x10FA

4347

R

10

Deg

INT16U

0–3600

H

Phase of harmonic 5 of IN (1)

0x10FB

4348

R

10

Deg

INT16U

0–3600

H

Phase of harmonic 7 of I1

0x10FC

4349

R

10

Deg

INT16U

0–3600

H

Phase of harmonic 7 of I2

0x10FD

4350

R

10

Deg

INT16U

0–3600

H

Phase of harmonic 7 of I3

0x10FE

4351

R

10

Deg

INT16U

0–3600

H

Phase of harmonic 7 of IN (1)

0x10FF

4352

R

10

Deg

INT16U

0–3600

H

Phase of harmonic 9 of I1

0x1100

4353

R

10

Deg

INT16U

0–3600

H

Phase of harmonic 9 of I2

0x1101

4354

R

10

Deg

INT16U

0–3600

H

Phase of harmonic 9 of I3

0x1102

4355

R

10

Deg

INT16U

0–3600

H

Phase of harmonic 9 of IN (1)

(1) Value is not available when the system type in register 3314 is 31. Refer to System Type.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?