DOCA0384EN-01

Energy Measurements

General Description

Energy measurements include:

  • active energy Ep

  • reactive energy Eq

  • apparent energy Es

  • active energy counted positively (EpIn) or negatively (EpOut), according to the configuration of register 3316 Power Flow Sign

  • reactive energy counted positively (EqIn) or negatively (EqOut), according to the configuration of register 3316 Power Flow Sign

  • active energy and reactive energy are accumulated according to the configuration of register 3324 (absolute mode by factory setting) Energy Accumulation Mode

The reset minimum/maximum command (command code = 46728) can reset the content of the energy measurement registers.

Address

Register

RW

X

Unit

Type

Range

A/E

Description

0x07CF–0x07D2

2000–2003

R-WC

1

kWh

MOD 10000

-1016 to +1016

E

Total active energy: Ep (1)

0x07D3–0x07D6

2004–2007

R-WC

1

kVARh

MOD 10000

-1016 to +1016

E

Total reactive energy: Eq (1)

0x07D7–0x07DA

2008–2011

R-WC

1

kWh

MOD 10000

-1016 to +1016

E

Active energy counted positively: EpIn

0x07DB–0x07DE

2012–2015

R-WC

1

kWh

MOD 10000

-1016 to +1016

E

Active energy counted negatively: EpOut

0x07DF–0x07E2

2016–2019

R-WC

1

kVARh

MOD 10000

-1016 to +1016

E

Reactive energy counted positively: EqIn

0x07E3–0x07E6

2020–2023

R-WC

1

kVARh

MOD 10000

-1016 to +1016

E

Reactive energy counted negatively: EqOut

0x07E7–0x07EA

2024–2027

R-WC

1

kVAh

MOD 10000

-1016 to +1016

E

Total apparent energy: Es

0x0BDD–0x0BDF

3038–3040

R

1

DATE

E

Date of last reset of energy meters

(1) Total active energy and total reactive energy are always counted positively with MicroLogic Active E control unit.

NOTE:
  • The MicroLogic Active E control unit screen displays positive values only up to 999 999 999 kWh. Above this value, MicroLogic Active E control unit screen displays 999 999 999 kWh.

  • MOD10000 format is explained in the Appendix.

The behavior is the same for reactive energy and apparent energy.

Energy per Phase

Address

Register

RW

Unit

Type

Range

A/E

Description

0xAD70–0xAD73

44401–44404

R-WC

Wh

INT64

E

Active energy delivered on phase 1 (into the load, counted positively)(1)

0xAD74–0xAD77

44405–44408

R-WC

Wh

INT64

E

Active energy received on phase 1 (out of the load, counted negatively)(1)

0xAD80–0xAD83

44417–44420

R-WC

Wh

INT64

E

Active energy delivered on phase 2 (into the load, counted positively)(1)

0xAD84–0xAD87

44421–44424

R-WC

Wh

INT64

E

Active energy received on phase 2 (out of the load, counted negatively)(1)

0xAD90–0xAD93

44433–44436

R-WC

Wh

INT64

E

Active energy delivered on phase 3 (into the load, counted positively)(1)

0xAD94–0xAD97

44437–44440

R-WC

Wh

INT64

E

Active energy received on phase 3 (out of the load, counted negatively)(1)

0xADA0–0xADA3

44449–44452

R-WC

VArh

INT64

E

Reactive energy delivered on phase 1 (into the load, counted positively)(1)

0xADA4–0xADA7

44453–44456

R-WC

VArh

INT64

E

Reactive energy received on phase 1 (out of the load, counted negatively)(1)

0xADB0–0xADB3

44465–44468

R-WC

VArh

INT64

E

Reactive energy delivered on phase 2 (into the load, counted positively)(1)

0xADB4–0xADB7

44469–44472

R-WC

VArh

INT64

E

Reactive energy received on phase 2 (out of the load, counted negatively)(1)

0xADC0–0xADC3

44481–44484

R-WC

VArh

INT64

E

Reactive energy delivered on phase 3 (into the load, counted positively)(1)

0xADC4–0xADC7

44485–44488

R-WC

VArh

INT64

E

Reactive energy received on phase 3 (out of the load, counted negatively)(1)

0xADD0–0xADD3

44497–44500

R-WC

VAh

INT64

E

Apparent energy on phase 1(1)

0xADD8–0xADDB

44505–44508

R-WC

VAh

INT64

E

Apparent energy on phase 2(1)

0xADE0–0xADE3

44513–44516

R-WC

VAh

INT64

E

Apparent energy on phase 3(1)

(1) Value reset with the reset energies command.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.