DOCA0384EN-01

Circuit Breaker Control Commands

Open Circuit Breaker

To open the circuit breaker, set the command registers as follows:

Address

Register

X

Unit

Type

Range

Description

0x1F3F

8000

INT16U

904

Command code = 904

0x1F40

8001

INT16U

10

Number of parameters (bytes) = 10

0x1F41

8002

INT16U

4353

Destination = 4353 (0x1101)

0x1F42

8003

INT16U

1

Security type of the command

0x1F43–

0x1F44

8004–

8005

OCTET STRING

Password of the command: Administrator or Operator user profile password

Close Circuit Breaker

To close the circuit breaker, set the command registers as follows:

Address

Register

X

Unit

Type

Range

Description

0x1F3F

8000

INT16U

905

Command code = 905

0x1F40

8001

INT16U

10

Number of parameters (bytes) = 10

0x1F41

8002

INT16U

4353

Destination = 4353 (0x1101)

0x1F42

8003

INT16U

1

Security type of the command

0x1F43–

0x1F44

8004–

8005

OCTET STRING

Password of the command: Administrator or Operator user profile password

Reset Circuit Breaker

To reset the circuit breaker, set the command registers as follows:

Address

Register

X

Unit

Type

Range

Description

0x1F3F

8000

INT16U

906

Command code = 906

0x1F40

8001

INT16U

10

Number of parameters (bytes) = 10

0x1F41

8002

INT16U

4353

Destination = 4353 (0x1101)

0x1F42

8003

INT16U

1

Security type of the command

0x1F43–0x1F44

8004–8005

OCTET STRING

Password of the command: Administrator or Operator user profile password

Enable/Inhibit a Circuit Breaker Close Order

To enable or inhibit a close order of the circuit breaker, set the command register as follows:

Address

Register

X

Unit

Type

Range

Description

0x1F3F

8000

INT16U

910

Command code = 910

0x1F40

8001

INT16U

13

Number of parameters (bytes) = 13

0x1F41

8002

INT16U

4353

Destination = 4353 (0x1101)

0x1F42

8003

INT16U

1

Security type of the command

0x1F43–

0x1F44

8004–

8005

OCTET STRING

Password of the command: Administrator or Operator user profile password

0x1F45

8006

INT16U

1

  • 0 = Enable close order

  • 1 = Inhibit close order

0x1F46

8007

INT16U

Origin of the command:

256 = command sent via communication interface (IFM or IFE)

Enable/Disable Automatic Reset

The user can read the automatic reset parameters at register 564 (bit 3).

To enable/disable automatic reset, set the command registers as follows:

Address

Register

X

Unit

Type

Range

Description

0x1F3F

8000

INT16U

42636

Command code = 42636

0x1F40

8001

INT16U

12

Number of parameters (bytes) = 12

0x1F41

8002

INT16U

4353

Destination = 4353 (0x1101)

0x1F42

8003

INT16U

1

Security type of the command

0x1F43–

0x1F44

8004–

8005

OCTET STRING

Password of the command: Administrator user profile password

0x1F45

8006

INT16U

0–1

0 = automatic reset is not enabled.

1 = automatic reset is enabled.

Enable/Disable Reset even if SDE

The user can read the reset parameters at register 564 (bit 4).

To enable/disable reset even if SDE, set the command registers as follows:

Address

Register

X

Unit

Type

Range

Description

0x1F3F

8000

INT16U

42637

Command code = 42637

0x1F40

8001

INT16U

12

Number of parameters (bytes) = 12

0x1F41

8002

INT16U

4353

Destination = 4353 (0x1101)

0x1F42

8003

INT16U

1

Security type of the command

0x1F43–

0x1F44

8004–

8005

OCTET STRING

Password of the command: Administrator user profile password

0x1F45

8006

INT16U

0–1

0 = reset is not enabled if SDE = 1.

1 = reset is enabled even if SDE = 1.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.