EIFE Interface Specific Commands
Reset EIFE Alarms
To reset EIFE interface alarms, set the command registers in the following way:
|
Address |
Register |
Unit |
Type |
Range |
Description |
|---|---|---|---|---|---|
|
0x1F3F |
8000 |
– |
INT16U |
41099 |
Command code = 41099 |
|
0x1F40 |
8001 |
– |
INT16U |
10 |
Number of parameters (bytes) = 10 |
|
0x1F41 |
8002 |
– |
INT16U |
8705 (0x2201) |
Destination = 8705 (0x2201) |
|
0x1F42 |
8003 |
– |
INT16U |
1 |
Security type of the command |
|
0x1F43– 0x1F44 |
8004– 8005 |
– |
OCTET STRING |
– |
Password of the command: Administrator or Operator user profile password |
Preset Cradle/Drawer Counters
To preset the cradle or drawer counters, set the command registers in the following way:
|
Address |
Register |
Unit |
Type |
Range |
Description |
|---|---|---|---|---|---|
|
0x1F3F |
8000 |
– |
INT16U |
41352 |
Command code = 41352 |
|
0x1F40 |
8001 |
– |
INT16U |
16 |
Number of parameters (bytes) = 16 |
|
0x1F41 |
8002 |
– |
INT16U |
8705 |
Destination = 8705 (0x2201) |
|
0x1F42 |
8003 |
– |
INT16U |
1 |
Security type of the command |
|
0x1F43– 0x1F44 |
8004– 8005 |
– |
OCTET STRING |
– |
Password of the command: Administrator or Operator user profile password |
|
0x1F45 |
8006 |
– |
INT16U |
0–65535 |
Connected counter reset/preset:
|
|
0x1F46 |
8007 |
– |
INT16U |
0–65535 |
Disconnected counter reset/preset:
|
|
0x1F47 |
8008 |
– |
INT16U |
0–65535 |
Test counter reset/preset:
|
Preset Regrease Timers
To preset regrease timers, set the command registers in the following way:
|
Address |
Register |
Unit |
Type |
Range |
Description |
|---|---|---|---|---|---|
|
0x1F3F |
8000 |
– |
INT16U |
41353 |
Command code = 41353 |
|
0x1F40 |
8001 |
– |
INT16U |
18 |
Number of parameters (bytes) = 18 |
|
0x1F41 |
8002 |
– |
INT16U |
8705 |
Destination = 8705 (0x2201) |
|
0x1F42 |
8003 |
– |
INT16U |
1 |
Security type of the command |
|
0x1F43– 0x1F44 |
8004– 8005 |
– |
OCTET STRING |
– |
Password of the command: Administrator or Operator user profile password |
|
0x1F45–0x1F46 |
8006–8007 |
– |
INT16U |
– |
Operating time since last grease maintenance
|
|
0x1F47–0x1F48 |
8008–8009 |
INT32U |
– |
Operating time since last move in rack in position (delay from last disconnection)
|
Get Events Command
To get events, set the command registers in the following way:
|
Address |
Register |
Unit |
Type |
Range |
Bit |
Description |
|---|---|---|---|---|---|---|
|
0x1F3F |
8000 |
– |
INT16U |
50560 |
– |
Command code = 50560 |
|
0x1F40 |
8001 |
– |
INT16U |
27 |
– |
Number of parameters (bytes) = 27 |
|
0x1F41 |
8002 |
– |
INT16U |
8705 (0x2201) |
– |
Destination = 8705 (0x2201) |
|
0x1F42 |
8003 |
– |
INT16U |
0 |
– |
Security type of the command |
|
0x1F43– 0x1F44 |
8004– 8005 |
– |
OCTET STRING |
– |
– |
Password of the command = 0 (no password required) |
|
0x1F45 |
8006 |
– |
– |
– |
– |
Reserved |
|
0x1F46 |
8007 |
– |
INT16U |
0, 2 |
– |
Requested get event method:
|
|
0x1F47–0x1F4A |
8008–8011 |
– |
– |
– |
– |
Reserved |
|
0x1F4B–0x1F4C |
8012–8013 |
– |
INT32U |
– |
– |
Requested event sequence number (for method 2 only) |
|
0x1F4D |
8014 |
– |
INT16U |
– |
– |
Requested event severity |
|
0–7 |
Reserved |
|||||
|
8 |
Low |
|||||
|
9 |
Medium |
|||||
|
10 |
High |
|||||
|
11–15 |
Reserved |
Events are returned to command registers in the following way:
|
Address |
Register |
Unit |
Type |
Range |
Bit |
Description |
|---|---|---|---|---|---|---|
|
0x1F53 |
8020 |
– |
INT16U |
50560 |
– |
Last command code |
|
0x1F54 |
8021 |
– |
INT16U |
– |
– |
Command status:
|
|
0x1F55 |
8022 |
– |
INT16U |
– |
– |
Number of bytes returned |
|
0x1F56 |
8023 |
– |
– |
– |
– |
Reserved |
|
0x1F57 |
8024 |
– |
INT16U |
0, 2 |
– |
Responded event requested method:
|
|
0x1F5E |
8031 |
– |
INT16U |
– |
– |
Responded event severity |
|
0–7 |
Reserved |
|||||
|
8 |
Low |
|||||
|
9 |
Medium |
|||||
|
10 |
High |
|||||
|
11–15 |
Reserved |
|||||
|
0x1F5F |
8032 |
– |
INT16U |
– |
– |
MSB: Number of events returned |
|
– |
LSB: Remaining events
|
|||||
|
0x1F60 |
8033 |
– |
INT16U |
1013-25630 |
– |
First event code |
|
0x1F61–0x1F64 |
8034–8037 |
– |
DATETIME |
– |
– |
Timestamp of the first event |
|
0x1F65 |
8038 |
– |
INT16U |
– |
– |
Timestamp quality of the first event |
|
0x1F66–0x1F67 |
8039–8040 |
– |
INT32U |
– |
– |
First event sequence number |
|
0x1F68 |
8041 |
– |
INT16U |
– |
– |
MSB: First event status
LSB: Reserved |
|
0x1F69 |
8042 |
– |
– |
– |
– |
Reserved |
|
0x1F6A |
8043 |
– |
INT16U |
– |
– |
First event severity |
|
0–7 |
Reserved |
|||||
|
8 |
Low |
|||||
|
9 |
Medium |
|||||
|
10 |
High |
|||||
|
11–15 |
Reserved |
|||||
|
0x1F6B–0x1F75 |
8044–8054 |
– |
INT16U |
– |
– |
Characteristics of event 2 (same as event 1) |
|
0x1F76–0x1F80 |
8055–8065 |
– |
INT16U |
– |
– |
Characteristics of event 3 (same as event 1) |
|
0x1F81– 0x1F8B |
8066–8076 |
– |
INT16U |
– |
– |
Characteristics of event 4 (same as event 1) |
|
0x1F8C–0x1F96 |
8077–8087 |
– |
INT16U |
– |
– |
Characteristics of event 5 (same as event 1) |
|
0x1F97–0x1FA1 |
8088–8098 |
– |
INT16U |
– |
– |
Characteristics of event 6 (same as event 1) |
|
0x1FA2–0x1FAC |
8099–8109 |
– |
INT16U |
– |
– |
Characteristics of event 7 (same as event 1) |
|
0x1FAD–0x1FB7 |
8110–8120 |
– |
INT16U |
– |
– |
Characteristics of event 8 (same as event 1) |
|
0x1FB8–0x1FC2 |
8121–8131 |
– |
INT16U |
– |
– |
Characteristics of event 9 (same as event 1) |
|
0x1FC3–0x1FCD |
8132–8142 |
– |
INT16U |
– |
– |
Characteristics of event 10 (same as event 1) |
Get Events Procedure
The command allows to get events by using one of the two following methods:
-
get the most recent events
-
get events before and up to an event sequence number. The event sequence number is an event identifier defined by the device, and is available among the event characteristics. It can be used to sort the events in chronological order.
The command allows to get 10 events maximum for one or several severity levels.
-
To get the 10 most recent events, use the method “get the most recent events”.
-
If there are more than 10 events, use the other method “get events before and up to an event sequence number” to get rest of the events.
Example: Read all events
The following diagram shows the steps to follow to read all events recorded in the device:
EIFE Interface Events
|
Event Code |
Description |
|---|---|
|
2304 (0x0900) |
Cradle position discrepancy |
|
2305 (0x0901) |
Cradle connected contact change |
|
2306 (0x0902) |
Cradle disconnected contact change |
|
2307 (0x0903) |
Cradle test contact change |
|
2308 (0x0904) |
Remove device from cradle and put it back |
|
2309 (0x0905) |
Cradle has reached its maximum number of operations |
|
2310 (0x0906) |
Remaining service life of cradle is below alarm threshold |
|
2311 (0x0907) |
New MicroLogic control unit has been detected |