Measurement Parameters
System Type
The setup ENVT (External Neutral Voltage Tap) presence command (command code = 46472) configures the content of the system type register.
|
Address |
Register |
RW |
X |
Unit |
Type |
Range |
Description |
|---|---|---|---|---|---|---|---|
|
0x0CF1 |
3314 |
R-WC |
– |
– |
INT16U |
30–41 |
System type |
Determining system type:
|
If... |
Then... |
Result |
|---|---|---|
|
the system type is 3-pole circuit breaker with external neutral current transformer and without external neutral voltage tap |
system type = 30 |
|
|
the system type is 3-pole circuit breaker without external neutral current transformer and without external neutral voltage tap |
system type = 31 |
|
|
the system type is 3-pole circuit breaker without external neutral current transformer and with external neutral voltage tap |
system type = 40 |
|
|
the system type is 3-pole circuit breaker with external neutral current transformer and external neutral voltage tap, or if the system type is 4-pole circuit breaker |
system type = 41 |
|
Quadrant Total
|
Address |
Register |
RW |
X |
Unit |
Type |
Range |
Description |
|---|---|---|---|---|---|---|---|
|
0x08C1 |
2242 |
R |
– |
– |
INT16U |
1–4 |
Quadrant total |
|
0x08C2 |
2243 |
R |
– |
– |
INT16U |
0–1 |
0 = lead 1 = lag |
Phase Rotation
The phase rotation setting command (command code = 47246) configures the content of the phase rotation register.
|
Address |
Register |
RW |
X |
Unit |
Type |
Range |
Description |
|---|---|---|---|---|---|---|---|
|
0X0CF2 |
3315 |
R-WC |
– |
– |
INT16U |
0–1 |
Phase rotation: 0 = I1, I2, I3 1 = I1, I3, I2 |
Power Flow Sign
The power flow sign command (command code = 47240) configures the content of the power flow sign register.
|
Address |
Register |
RW |
X |
Unit |
Type |
Range |
Description |
|---|---|---|---|---|---|---|---|
|
0x0CF3 |
3316 |
R-WC |
– |
– |
INT16U |
0–1 |
Power flow sign: 0 = the active power flows from upstream (top) to downstream (bottom) (factory setting). 1 = the active power flows from downstream (bottom) to upstream (top). |
Power Factor Sign
The power factor sign configuration command (command code = 47241) configures the content of the power factor sign register.
|
Address |
Register |
RW |
X |
Unit |
Type |
Range |
Description |
|---|---|---|---|---|---|---|---|
|
0x0CF5 |
3318 |
R-WC |
– |
– |
INT16U |
0–2 |
Sign convention for the power factor and the fundamental power factor (cosϕ): 0 = IEC convention 2 = IEEE convention (factory setting) |
Energy Accumulation Mode
The energy accumulation mode configuration command (command code = 47242) configures the content of the energy accumulation mode register.
|
Address |
Register |
RW |
X |
Unit |
Type |
Range |
Description |
|---|---|---|---|---|---|---|---|
|
0x0CFB |
3324 |
R-WC |
– |
– |
INT16U |
0–1 |
Energy accumulation mode: 0 = absolute accumulation (factory setting) Ep = EpIn + EpOut Eq = EqIn + EqOut 1 = signed accumulation Ep = EpIn – EpOut Eq = EqIn – EqOut |
Demand Time
The current demand configuration command (command code 47243) configures the content of register 3352.
The power demand configuration command (command code 47244) configures the content of registers 3354 and 3355.
For more information regarding the demand calculation method, refer to the following guides in Related Documents at the beginning of this guide:
-
DOCA0188•• ComPacT NSX MicroLogic 5/6/7 Trip Units - User Guide
-
48940-312-01 - MicroLogic 5 and 6 Electronic Trip Units for PowerPacT H-, J-, and L-Frame Circuit Breakers - User Guide
|
Address |
Register |
RW |
X |
Unit |
Type |
Range |
Description |
|---|---|---|---|---|---|---|---|
|
0x0D17 |
3352 |
R-WC |
– |
min |
INT16U |
5–60 |
Duration of the current demand calculation window, adjustable in steps of 1 minute. The factory setting is 15 minutes. |
|
0x0D19 |
3354 |
R-WC |
– |
– |
INT16U |
0–5 |
Power demand calculation method (window type): 0 = sliding (factory setting) 2 = block 5 = synchronized to communication |
|
0x0D1A |
3355 |
R-WC |
– |
min |
INT16U |
5–60 |
Duration of the power demand calculation window, adjustable in steps of 1 minute. The factory setting is 15 minutes. |
Nominal Voltage
The setup nominal voltage Vn display command (command code = 47245) configures the content of the nominal voltage register.
|
Address |
Register |
RW |
X |
Unit |
Type |
Range |
Description |
|---|---|---|---|---|---|---|---|
|
0x258F |
9616 |
R-WC |
1 |
V |
INT16U |
0–65535 |
Nominal voltage Vn. Factory setting = 400 V |