Circuit Breaker Control Commands
Open Circuit Breaker
DANGER |
|---|
|
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
Failure to follow these instructions will result in death or serious injury.
|
To open the circuit breaker, the user must set up the command registers as follows:
|
Address |
Register |
X |
Unit |
Type |
Range |
A/E |
Description |
|---|---|---|---|---|---|---|---|
|
0x1F3F |
8000 |
– |
– |
INT16U |
904 |
A/E |
Command code = 904 |
|
0x1F40 |
8001 |
– |
– |
INT16U |
10 |
A/E |
Number of parameters (bytes) = 10 |
|
0x1F41 |
8002 |
– |
– |
INT16U |
4609 |
A/E |
Destination = 4609 (0x1201) |
|
0x1F42 |
8003 |
– |
– |
INT16U |
1 |
A/E |
Security type of the command |
|
0x1F43–0x1F44 |
8004–8005 |
– |
– |
OCTET STRING |
– |
A/E |
Password of the command = 0 (no password required) |
Close Circuit Breaker
DANGER |
|---|
|
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
Failure to follow these instructions will result in death or serious injury.
|
To close the circuit breaker, the user must set up the command registers as follows:
|
Address |
Register |
X |
Unit |
Type |
Range |
A/E |
Description |
|---|---|---|---|---|---|---|---|
|
0x1F3F |
8000 |
– |
– |
INT16U |
905 |
A/E |
Command code = 905 |
|
0x1F40 |
8001 |
– |
– |
INT16U |
10 |
A/E |
Number of parameters (bytes) = 10 |
|
0x1F41 |
8002 |
– |
– |
INT16U |
4609 |
A/E |
Destination = 4609 (0x1201) |
|
0x1F42 |
8003 |
– |
– |
INT16U |
1 |
A/E |
Security type of the command |
|
0x1F43–0x1F44 |
8004–8005 |
– |
– |
OCTET STRING |
– |
A/E |
Password of the command = 0 (no password required) |
DANGER