DOCA0384EN-01

List of MicroLogic X Control Unit Protection Commands with Session and Error Codes

List of Commands

The MicroLogic X control unit protection commands with session are performed by the command interface. They are grouped by their functions and types:

In the MicroLogic X control unit registers:

  • RC indicates the registers that can be read by a get command

  • WC indicates the registers that can be written by a set and reset command

Error Codes

Error codes generated by MicroLogic X control units are the generic error codes.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?