DOCA0384EN-01

List of MicroLogic A/E/P/H Trip Unit Commands and Error Codes

List of Commands

The following table lists the available MicroLogic A/E/P/H trip unit commands, their corresponding command codes, and user profiles. Follow the command execution procedures accordingly Executing a Command:

Command

Command Code

User Profile

Set up ENVT presence Set Up ENVT Presence

46472

Administrator

Reset minimum/maximum Reset Minimum/Maximum

46728

Administrator or Operator

Power flow sign configuration Power Flow Sign Configuration

47240

Administrator

Power factor sign configuration Power Factor Sign Configuration

47241

Administrator

Energy accumulation mode configuration Energy Accumulation Mode Configuration

47242

Administrator

Current demand configuration Current Demand Configuration

47243

Administrator

Power demand configuration Power Demand Configuration

47244

Administrator

Set up nominal voltage Vn display Set Up Nominal Primary Voltage Vn Display

47245

Administrator

For additional commands related to protection settings, refer to MasterPacT Modbus Legacy User Guide.

Error Codes

Error codes generated by MicroLogic A/E/P/H trip units are the generic error codes.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?