DOCA0384EN-01

List of BSCM Modbus SL/ULP Module Commands and Error Codes

List of Commands

The following table lists the available BSCM Modbus SL/ULP module commands, their corresponding command codes and user profiles. Follow the command execution procedures.

Command

Command code

User profile

Open circuit breaker

904

Administrator or Operator

Close circuit breaker

905

Administrator or Operator

Reset circuit breaker

906

Administrator or Operator

Enable/inhibit close order

910

Administrator or Operator

Enable/disable automatic reset

42636

Administrator

Enable/disable reset even if SDE

42637

Administrator

Preset counters

42638

Administrator

Set up thresholds

42639

Administrator

Get current time

768

No password required

Set absolute time

769

No password required

Read IMU name and location

1024

No password required

Write IMU name and location

1032

Administrator

Set validity duration of data

41868

Administrator, Services, Engineer, or Operator

Error Codes

Error codes generated by the BSCM Modbus SL/ULP module commands are returned in register 8021. In addition to generic error codes, the BSCM Modbus SL/ULP module commands generate the following error codes:

Error Code

Description

4363 (0x110B)

BSCM Modbus SL/ULP module is out of order.

4503 (0x1197)

Circuit breaker is tripped. It must be reset before the command.

4504 (0x1198)

Circuit breaker is already closed.

4505 (0x1199)

Circuit breaker is already open.

4506 (0x119A)

Circuit breaker is already reset.

4507 (0x119B)

Actuator is in manual mode. Remote commands are not allowed.

4508 (0x119C)

Actuator is not present.

4510 (0x119E)

A previous command is still in progress.

4511 (0x119F)

Reset command is forbidden when SDE is set.

4512 (0x11A0)

Inhibit close order is enabled.

Any other positive error code indicates an internal error.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?