DOCA0384EN-01

Trip History

General Description

The trip history registers describe the last 10 encountered trips. The trip history format corresponds to a series of 10 records saved in a FIFO (first in first out) stack. The last record erases the oldest. Each record is composed of 20 registers describing one trip.

Register 9098 returns the number of faults recorded in the trip history (FIFO).

Register 9099 returns the value of the pointer for the last fault recorded in the trip history.

Example:

If the register 9098 = 10 and the register 9099 = 5, then the last fault recorded is the trip record 5.

In this case, the last but one is the alarm record 4.

NOTE:
  • The contacts must be inspected each time the counter reaches a hundred mark.

  • The message Not available or circuit breaker type not defined is displayed if the characteristics of the circuit breaker have not been defined. In this case, see Breaker selection in the MicroLogic setup menu on the MicroLogic HMI, in registers 9846–9853.

Address

Register

RW

X

Unit

Type

Range

A/E/P/H

Description

0x2385

9094

R

1

%

INT16U

0–32767

P/H

Phase 1 contact wear indicator (1)

0x2386

9095

R

1

%

INT16U

0–32767

P/H

Phase 2 contact wear indicator (1)

0x2387

9096

R

1

%

INT16U

0–32767

P/H

Phase 3 contact wear indicator (1)

0x2388

9097

R

1

%

INT16U

0–32767

P/H

Neutral contact wear indicator (1)

0x2389

9098

R

INT16U

0–10

P/H

Number of alarms recorded in the trip history (FIFO)

0x238A

9099

R

INT16U

0–9

P/H

Value of the pointer for last alarm recorded in the trip history

(1) Factory setting = 0x8000.

Trip Record Number

A read request of 20x(n) registers is necessary to read the last n trip records, where 20 is the number of registers for each trip record.

For example, a read request of 20x3 = 60 registers is necessary to read the last 3 trip records of the trip history:

  • The first 20 registers describe the first trip record.

  • The next 20 registers describe the second trip record.

  • The last 20 registers describe the third trip record.

Address

Register

Description

0x238B–0x239E

9100–9119

Trip record 0

0x239F–0x23B2

9120–9139

Trip record 1

0x23B3–0x23C6

9140–9159

Trip record 2

0x23C7–0x23DA

9160–9179

Trip record 3

0x23DB–0x23EE

9180–9199

Trip record 4

0x23EF–0x2402

9200–9219

Trip record 5

0x2403–0x2416

9220–9239

Trip record 6

0x2417–0x242A

9240–9259

Trip record 7

0x242B–0x243E

9260–9279

Trip record 8

0x243F–0x2452

9280–9299

Trip record 9

Trip Record

A read request of 20 registers is necessary to read a trip record.

The order and the description of the trip record registers are the same as that of the trip record 0:

Trip Record 0

Address

Register

RW

X

Unit

Type

Range

A/E/P/H

Description

0x238B–0x238E

9100–9103

R

XDATE

E/P/H

Trip date

0x238F

9104

R

INT16U

1000–1030

E/P/H

Trip code

0x2390–0x2391

9105–9106

R

MOD 10000

P/H

Value of protection setting that caused alarm activation

0x2392

9107

R

INT16U

P/H

Value of time delay that caused trip

0x2393

9108

R

INT16U

0–16000

P/H

Trip current phase 1 (1)

0x2394

9109

R

INT16U

0–16000

P/H

Trip current phase 2 (1)

0x2395

9110

R

INT16U

0–16000

P/H

Trip current phase 3 (1)

0x2396

9111

R

INT16U

0–16000

P/H

Trip current neutral (1)

0x2397

9112

R

P/H

New value of contact-wear indicator following a trip (2)

0x2398–0x2399

9113–9114

Reserved

0x239A–0x239E

9115–9119

Reserved

(1) Expressed as x 0.1 of In (rated current).

(2) The trip unit records one indicator per contact. Here, only the value for the most worn contact is given. See registers 9094 to 9097.

Trip Codes

Trip Code

Description

1000 (0x03E8)

Trip due to long-time protection Ir

1001 (0x03E9)

Trip due to short-time protection Isd

1002 (0x03EA)

Trip due to instantaneous protection Ii

1003 (0x03EB)

Trip due to ground-fault protection Ig

1004 (0x03EC)

Trip due to earth-leakage protection IΔn

1005 (0x03ED)

Trip due to integrated instantaneous protection I >>

10061007 (0x03EE0x03EF)

Reserved

1008 (0x03F0)

Trip due to advanced protection

1009 (0x03F1)

Trip due to extended advanced protection

10101015 (0x03F20x03F7)

Reserved

1016 (0x3F8)

Current unbalance

1017 (0x3F9)

I1 maximum demand

1018 (0x3FA)

I2 maximum demand

1019 (0x3FB)

I3 maximum demand

1020 (0x3FC)

IN maximum demand

1021 (0x3FD)

Undervoltage

1022 (0x3FE)

Overvoltage

1023 (0x3FF)

Voltage unbalance

1024 (0x400)

Reserved

1025 (0x401)

Reverse power

1026 (0x402)

Underfrequency

1027 (0x403)

Overfrequency

1028 (0x404)

Phase rotation

1029 (0x405)

Current load shedding

1030 (0x406)

Power load shedding

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?