DOCA0384EN-01

Maintenance Metering Event Log

General Description

The system stores the events that concern the maintenance metering manager (counter reset, and so on) in file number 12.

This file is made up of 20 records and each record is made up of six registers.

File Header

The following table describes the file header content:

Address

Register

RW

X

Unit

Type

Range

A/E/P/H

Description

0x1C3B

7228

RW

INT16U

H

File status:

0x0000 = file disabled

0xFFFF = file enabled (factory setting)

0x1C3C

7229

R

INT16U

H

Type of file:

12 = maintenance metering event log

0x1C3D

7230

R

1

INT16U

H

Size of a file = 20 records

0x1C3E

7231

R

1

INT16U

H

Size of a record = 6 registers

0x1C3F

7232

R

INT16U

1

H

File filling mode:

1 = disabled if log is full

File Status

The following table describes the file status content:

Address

Register

RW

X

Unit

Type

Range

A/E/P/H

Description

0x1C4B

7244

R

1

INT16U

H

Size of a file = 20 records

0x1C4C

7245

R

1

INT16U

H

Size of a record = 6 registers

0x1C4D

7246

R

1

INT16U

H

0x0000 = file OK

0x000A = record size smaller than expected

0x0014 = record size larger than expected

0x001E = insufficient memory

0x00FA = internal error

0x00FD = corrupted allocation table

0x00FE = configuration zero

0x00FF = invalid configuration

0xFC00 = invalid file number

0xFD00 = invalid record number

0xFE00 = file not supported

0xFF00 = cannot allocate file

0x1C4E

7247

R

1

INT16U

20

H

Number of records in the file = 20

0x1C4F

7248

R

1

INT16U

1

H

Sequence number of first record in the file (the oldest) = 1

0x1C50

7249

R

1

INT16U

20

H

Sequence number of last record in the file (the most recent) = 20

0x1C51– 0x1C53

7250– 7252

R

DATE

H

Date the last file was reset.

Factory setting = 0x8000 0x8000 0x8000

Maintenance Metering Event Record

The maintenance metering event log has a fixed number of records and all record has a fixed number of registers:

Record Number

Registers

Type

Description

1

1–3

DATE

Date/time of last counter reset

4

INT16U

Number of minimum resets

5–6

Reserved

2

1–3

DATE

Date/time of last counter reset

4

INT16U

Number of maximum resets

5–6

Reserved

3

1–3

DATE

Date/time of last counter reset

4

INT16U

Number of peak current demand resets

5–6

Reserved

4

1–3

DATE

Date/time of last counter reset

4

INT16U

Number of peak power demand resets

5–6

Reserved

5

1–3

DATE

Date/time of last counter reset

4

INT16U

Number of energy resets

5–6

Reserved

6–20

1–6

Reserved

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?