DOCA0384EN-01

Alarm History

General Description

The alarm history registers describe the last 10 alarms. The alarm history format corresponds to a series of 10 records. Each record is composed of 5 registers describing one alarm.

The alarm history registers return 32768 (0x8000) when they are not used.

Record Number

A read request of 5x(n) registers is necessary to read the last n alarm records, where 5 is the number of registers for each alarm record.

For example, a read request of 5 x 3 = 15 registers is necessary to read the last 3 alarm records of the alarm history:

  • The first 5 registers describe the first alarm record (most recent alarm).

  • The next 5 registers describe the second alarm record.

  • The last 5 registers describe the third alarm record.

Address

Register

Description

0x1663–0x1667

5732–5736

Alarm record 1 (most recent alarm)

0x1668–0x166C

5737–5741

Alarm record 2

0x166D–0x1671

5742–5746

Alarm record 3

0x1672–0x1676

5747–5751

Alarm record 4

0x1677–0x167B

5752–5756

Alarm record 5

0x167C–0x1680

5757–5761

Alarm record 6

0x1681–0x1685

5762–5766

Alarm record 7

0x1686–0x168A

5767–5771

Alarm record 8

0x168B–0x168F

5772–5776

Alarm record 9

0x1690–0x1694

5777–5781

Alarm record 10 (oldest alarm)

Alarm Record

A read request of 5 registers is necessary to read an alarm record.

The order and the description of the alarm records registers are the same as that of the alarm record 1:

Alarm Record 1 (Most Recent Alarm)

Address

Register

RW

X

Unit

Type

Range

Description

0x1663

5732

R

1

INT16U

0–65535

Alarm code (see next paragraph)

0x1664–

0x1666

5733–

5735

R

ULP DATE

Date and time of alarm Data Type: ULP DATE

0x1667

5736

R

1

INT16U

1–2

Event type

MSB = 0 (reserved)

Event occurrence: LSB = 1

Event completion: LSB = 2

Alarm Codes

Alarm Code

Description

201 (0x00C8)

User-defined alarm 201

202 (0x00C9)

User-defined alarm 202

203 (0x00CA)

User-defined alarm 203

204 (0x00CB)

User-defined alarm 204

205 (0x00CC)

User-defined alarm 205

206 (0x00CD)

User-defined alarm 206

207 (0x00CE)

User-defined alarm 207

208 (0x00CF)

User-defined alarm 208

209 (0x00D0)

User-defined alarm 209

210 (0x00D1)

User-defined alarm 210

1013 (0x03F4)

Long-time protection Ir pre-alarm (PAL Ir)

1014 (0x03F5)

Ground-fault protection Ig pre-alarm (PAL Ig)

1015 (0x03F6)

Earth-leakage protection IΔn pre-alarm (PAL IΔn)

The list of the predefined alarms from which the user can choose the 10 user-defined alarms is available at User-Defined Alarms.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?