DOCA0384EN-01

Counter Commands

Preset Counters

The user can read the values of the counters from registers 571 to 578.

To preset the counters, the user must set up the command registers as follows:

Address

Register

X

Unit

Type

Range

Description

0x1F3F

8000

INT16U

42638

Command code = 42638

0x1F40

8001

INT16U

22

Number of parameters (bytes) = 22

0x1F41

8002

INT16U

4353

Destination = 4353 (0x1100)

0x1F42

8003

INT16U

1

Security type of the command

0x1F43–

0x1F44

8004–

8005

OCTET STRING

Password of the command: Administrator user profile password

0x1F45

8006

1

INT16U

0–65535

0–65534 = preset value of the OF counter

65535 = do not preset the OF counter

0x1F46

8007

1

INT16U

0–65535

0–65534 = preset value of the SD counter

65535 = do not preset the SD counter

0x1F47

8008

1

INT16U

0–65535

0–65534 = preset value of the SDE counter

65535 = do not preset the SDE counter

0x1F48

8009

1

INT16U

0–65535

0–65534 = preset value of the open circuit breaker command counter

65535 = do not preset the open circuit breaker command counter

0x1F49

8010

1

INT16U

0–65535

0–65534 = preset value of the close circuit breaker command counter

65535 = do not preset the close circuit breaker command counter

0x1F4A

8011

1

INT16U

0–65535

0–65534 = preset value of the reset circuit breaker command counter

65535 = do not preset the reset circuit breaker command counter

Set Up Thresholds

The user can read the values of the thresholds from registers 581 to 582.

To set up the thresholds, the user must set up the command registers as follows:

Address

Register

X

Unit

Type

Range

Description

0x1F3F

8000

INT16U

42639

Command code = 42639

0x1F40

8001

INT16U

22

Number of parameters (bytes) = 22

0x1F41

8002

INT16U

4353

Destination = 4353 (0x1100)

0x1F42

8003

INT16U

1

Security type of the command

0x1F43–

0x1F44

8004–

8005

OCTET STRING

Password of the command: Administrator user profile password

0x1F45

8006

1

INT16U

0–65535

0–65534 = value of the OF counter threshold

65535 = do not change the OF counter threshold

0x1F46

8007

1

INT16U

65535

65535 (no threshold is set up for the SD counter)

0x1F47

8008

1

INT16U

65535

65535 (no threshold is set up for the SDE counter)

0x1F48

8009

1

INT16U

65535

65535 (no threshold is set up for the open circuit breaker command counter)

0x1F49

8010

1

INT16U

0–65535

0–65534 = value of the close circuit breaker command counter threshold

65535 = do not change close circuit breaker command counter threshold

0x1F4A

8011

1

INT16U

65535

65535 (no threshold is set up for the reset circuit breaker command counter)

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.