DOCA0384EN-01

Modbus Exception Codes

Exception Responses

Exception responses from either the client or a server can result from data processing errors. One of the following events can occur after a request from the client:

  • If the server receives the request from the client without a communication error and can handle the request correctly, it returns a normal response.

  • If the server does not receive the request from the client due to a communication error, it does not return a response. The client program eventually processes a timeout condition for the request.

  • If the server receives the request from the client but detects a communication error, it does not return a response. The client program eventually processes a timeout condition for the request.

  • If the server receives the request from the client without a communication error, but cannot handle it (for example, the request is to read a register that does not exist), the server returns an exception response to inform the client of the nature of the error.

Exception Frame

The server sends an exception frame to the client to report an exception response. An exception frame is composed of 4 fields:

Field

Definition

Size

Description

1

Server number

1 byte

Destination of the request

  • 1–247: unique destination

2

Exception function code

1 byte

Request function code + 128 (0x80)

3

Exception code

n bytes

See next paragraph

4

CRC error checking

2 bytes

CRC16 (to check the integrity of the Modbus frame)

Exception Codes

The exception response frame has two fields that differentiate it from a normal response frame:

  • The exception function code of the exception response is equal to the function code of the original request plus 128 (0x80).

  • The exception code depends on the communication error that the server encounters.

The following table describes the exception codes handled by the communication interface:

Exception Code

Name

Description

01 (0x01)

Illegal function

The function code received in the request is not an authorized action for the server. The server may be in the wrong state to process a specific request.

02 (0x02)

Illegal data address

The data address received by the server is not an authorized address for the server.

03 (0x03)

Illegal data value

The value in the request data field is not an authorized value for the server.

04 (0x04)

Server device failure

The server fails to perform a requested action because of an unrecoverable error.

05 (0x05)

Acknowledge

The server accepts the request but needs a long time to process it.

06 (0x06)

Server device busy

The server is busy processing another command. The client must send the request once the server is available.

07 (0x07)

Negative acknowledgment

The server cannot perform the programming request sent by the client.

08 (0x08)

Memory parity error

The server detects a parity error in the memory when attempting to read extended memory.

10 (0x0A)

Gateway path unavailable

The gateway is overloaded or not correctly configured.

11 (0x0B)

Gateway target device failed to respond

The server is not present on the network.

Illegal Data Address

This guide describes the registers available for each IMU module with the latest firmware version. When a register described in the guide is not implemented in an IMU module that has an old firmware version, an exception response is returned with the exception code 02 (0x02), illegal data address.

You can update the firmware of the IMU modules by using EcoStruxure Power Commission software.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?