Legacy Dataset Common Registers
Circuit Breaker Status Register
|
Address |
Register |
RW |
Unit |
Type |
Range |
A/E |
A/E/P/H |
Active |
X |
Bit |
Description |
|---|---|---|---|---|---|---|---|---|---|---|---|
|
0x2EDF |
12000 |
R |
– |
INT16U |
– |
A/E |
A/E/P/H |
A/E |
X |
– |
Validity of each bit in the circuit breaker status register. |
|
0x2EE0 |
12001 |
R |
– |
INT16U |
– |
A/E |
A/E/P/H |
A/E |
X |
– |
Circuit breaker status register |
|
A/E |
A/E/P/H |
A/E |
X |
0 |
OF status indication contact 0 = The circuit breaker is open. 1 = The circuit breaker is closed. |
||||||
|
A/E |
A/E/P/H |
A/E |
X |
1 |
SD trip indication contact 0 = Circuit breaker is not tripped. 1 = Circuit breaker is tripped due to electrical fault, shunt trip or push-to-trip. Bit always equal to 0 for MasterPacT NT/NW, ComPacT NS and PowerPacT P- and R-frame circuit breakers with motor mechanism. |
||||||
|
A/E |
A/E/P/H |
A/E |
X |
2 |
SDE fault trip indication contact 0 = Circuit breaker is not tripped on electrical fault. 1 = Circuit breaker is tripped due to electrical fault (including ground-fault test and earth-leakage test). |
||||||
|
– |
A/E/P/H |
A/E |
X |
3 |
CH spring charged contact (only with MasterPacT) 0 = Spring discharged 1 = Spring charged Bit always equal to 0 for ComPacT NS and PowerPacT P- and R-frame circuit breakers with motor mechanism. |
||||||
|
– |
– |
– |
– |
4 |
Reserved |
||||||
|
– |
A/E/P/H |
A/E |
X |
5 |
PF ready to close contact (only with MasterPacT) 0 = Not ready to close 1 = Ready to close Bit always equal to 0 for ComPacT NS and PowerPacT P- and R-frame circuit breakers with motor mechanism. |
||||||
|
– |
A/E/P/H |
A/E |
X |
6 |
Distinction between ComPacT NS,PowerPacT P- and R-frame and MasterPacT NT/NW 0 = ComPacT NS or PowerPacT P- and R-frame 1 = MasterPacT NT/NW |
||||||
|
– |
– |
– |
– |
7–14 |
Reserved |
||||||
|
A/E |
– |
– |
X |
15 |
Data availability If this bit is set at 1, all other bits of the register are not significant. |
IO Status Registers
|
Address |
Register |
RW |
Unit |
Type |
Range |
A/E |
A/E/P/H |
Active |
X |
Bit |
Description |
|---|---|---|---|---|---|---|---|---|---|---|---|
|
0x2EE1 |
12002 |
R |
– |
INT16U |
– |
A/E |
A/E/P/H |
A/E |
X |
– |
Status IO 1 |
|
0 |
Input 1 status
|
||||||||||
|
1 |
Input 2 status
|
||||||||||
|
2 |
Input 3 status
|
||||||||||
|
3 |
Input 4 status
|
||||||||||
|
4 |
Input 5 status
|
||||||||||
|
5 |
Input 6 status
|
||||||||||
|
6 |
Output 1 status
|
||||||||||
|
7 |
Output 2 status
|
||||||||||
|
8 |
Output 3 status
|
||||||||||
|
9–14 |
Reserved |
||||||||||
|
15 |
Data availability If this bit is set at 1, all other bits of the register are not significant. |
||||||||||
|
0x2EE2 |
12003 |
R |
– |
INT16U |
– |
A/E |
A/E/P/H |
A/E |
X |
– |
Status IO 2 |
|
0 |
Input 1 status
|
||||||||||
|
1 |
Input 2 status
|
||||||||||
|
2 |
Input 3 status
|
||||||||||
|
3 |
Input 4 status
|
||||||||||
|
4 |
Input 5 status
|
||||||||||
|
5 |
Input 6 status
|
||||||||||
|
6 |
Output 1 status
|
||||||||||
|
7 |
Output 2 status
|
||||||||||
|
8 |
Output 3 status
|
||||||||||
|
9–14 |
Reserved |
||||||||||
|
15 |
Data availability If this bit is set at 1, all other bits of the register are not significant. |
Tripping Cause
The tripping cause register provides information about the cause of the trip for the standard protection functions. When a tripping cause bit is at 1 in the tripping cause register, it indicates that a trip has occurred and has not been reset.
-
For MicroLogic trip units for ComPacT NSX and PowerPacT H-, J-, and L-frame circuit breakers, the tripping cause bit is reset by pressing the OK key (keypad of the MicroLogic trip unit) twice (validation and confirmation).
-
For MicroLogic A/E/P/H trip units for MasterPacT NT/NW, ComPacT NS and PowerPacT P- and R-frame circuit breakers, the tripping cause bit is reset as soon as the circuit breaker is closed again.
-
For MicroLogic X control units for MasterPacT MTZ circuit breakers, the tripping cause bit is reset by pressing the test/reset button (located beside the trip cause LEDs on the MicroLogic X control unit). Press and hold the button for 3 to 15 seconds to reset all the trip causes.
-
For MicroLogic Active control units for MasterPacT MTZ circuit breakers, the tripping cause bit is reset by pressing the
button located on the front face of the MicroLogic Active control unit. Press and hold the
button for more than 3 seconds to reset all the trip causes.
|
Address |
Register |
RW |
Unit |
Type |
Range |
A/E |
A/E/P/H |
Active |
X |
Bit |
Description |
|---|---|---|---|---|---|---|---|---|---|---|---|
|
0x2EE3 |
12004 |
R |
– |
INT16U |
– |
A/E |
A/E/P/H |
A/E |
X |
– |
Tripping cause for the standard protection functions |
|
A/E |
A/E/P/H |
A/E |
X |
0 |
Long-time protection Ir |
||||||
|
A/E |
P/H |
A/E |
X |
1 |
Short-time protection Isd |
||||||
|
– |
A/E |
A/E |
X |
1 |
Short-time protection Isd or Instantaneous protection Ii |
||||||
|
A/E |
P/H |
A/E |
X |
2 |
Instantaneous protection Ii |
||||||
|
A/E |
A/E/P/H |
A/E |
X |
3 |
Ground-fault protection Ig |
||||||
|
E |
A/P/H |
A/P/H |
X |
4 |
Earth-leakage protection IΔn |
||||||
|
A/E |
A/E/P/H |
A/E |
X |
5 |
Integrated instantaneous protection (SELLIM and DIN/DINF) for:
|
||||||
|
A/E |
– |
– |
X |
6 |
Internal failure (STOP) |
||||||
|
– |
A/E |
A/E |
– |
Other protections or integrated instantaneous protection |
|||||||
|
– |
P/H |
E |
– |
Internal failure (temperature) |
|||||||
|
– |
A/E/P/H |
A/E |
– |
7 |
Internal failure (overvoltage) |
||||||
|
– |
P/H |
E |
X |
8 |
Other protection (see register 12005) |
||||||
|
E |
– |
– |
– |
9 |
Instantaneous with earth-leakage protection on the trip unit. |
||||||
|
E |
– |
– |
– |
10 |
Unbalance motor protection |
||||||
|
E |
– |
– |
– |
11 |
Jam motor protection |
||||||
|
E |
– |
– |
– |
12 |
Underload motor protection |
||||||
|
E |
– |
– |
– |
13 |
Long-start motor protection |
||||||
|
A/E |
– |
– |
– |
14 |
Reflex tripping protection |
||||||
|
A/E |
A/E/P/H |
A/E |
X |
15 |
If this bit is at 1, bits 0 to 14 are not valid. |
||||||
|
0x2EE4 |
12005 |
R |
– |
INT16U |
– |
– |
P/H |
E |
X |
– |
Tripping causes for the advanced protection functions |
|
– |
P/H |
– |
– |
0 |
Current unbalance |
||||||
|
– |
P/H |
– |
– |
1 |
Overcurrent on phase 1 |
||||||
|
– |
P/H |
– |
– |
2 |
Overcurrent on phase 2 |
||||||
|
– |
P/H |
– |
– |
3 |
Overcurrent on phase 3 |
||||||
|
– |
P/H |
– |
– |
4 |
Overcurrent on Neutral |
||||||
|
– |
P/H |
E |
X |
5 |
Undervoltage |
||||||
|
– |
P/H |
E |
X |
6 |
Overvoltage |
||||||
|
– |
P/H |
– |
– |
7 |
Voltage unbalance |
||||||
|
– |
P/H |
– |
– |
8 |
Overpower |
||||||
|
– |
P/H |
– |
X |
9 |
Reverse power |
||||||
|
– |
P/H |
– |
X |
10 |
Underfrequency |
||||||
|
– |
P/H |
– |
X |
11 |
Overfrequency |
||||||
|
– |
P/H |
– |
– |
12 |
Phase rotation |
||||||
|
– |
P/H |
– |
– |
13 |
Load shedding based on current |
||||||
|
– |
P/H |
– |
– |
14 |
Load shedding based on power |
||||||
|
– |
P/H |
E |
X |
15 |
If this bit is at 1, bits 0 to 14 are not valid. |
||||||
|
0x2EE5– 0x2EE6 |
12006– 12007 |
– |
– |
– |
– |
– |
– |
– |
– |
– |
Reserved |
Overrun of the Protection Setpoints
The alarm setpoint registers provide information about overrun of the standard and advanced protection setpoints. A bit is at 1 once a setpoint overrun has occurred, even if the time delay has not expired.
|
Address |
Register |
RW |
Unit |
Type |
Range |
A/E |
A/E/P/H |
Active |
X |
Bit |
Description |
|---|---|---|---|---|---|---|---|---|---|---|---|
|
0x2EE7 |
12008 |
R |
– |
INT16U |
– |
A/E |
P/H |
A/E |
– |
– |
Overrun of the standard protection setpoints |
|
A/E |
P/H |
A/E |
– |
0 |
Long-time protection pick-up |
||||||
|
– |
– |
– |
– |
1–14 |
Reserved |
||||||
|
A/E |
P/H |
E |
– |
15 |
If this bit is at 1, bits 0 to 14 are not valid. |
||||||
|
0x2EE8 |
12009 |
R |
– |
INT16U |
– |
– |
P/H |
E |
– |
– |
Overrun of the advanced protection setpoints |
|
– |
P/H |
E |
– |
0 |
Current unbalance |
||||||
|
– |
P/H |
E |
– |
1 |
Maximum current on phase 1 |
||||||
|
– |
P/H |
E |
– |
2 |
Maximum current on phase 2 |
||||||
|
– |
P/H |
E |
– |
3 |
Maximum current on phase 3 |
||||||
|
– |
P/H |
E |
– |
4 |
Maximum current on the neutral |
||||||
|
– |
P/H |
E |
– |
5 |
Minimum voltage |
||||||
|
– |
P/H |
E |
– |
6 |
Maximum voltage |
||||||
|
– |
P/H |
– |
– |
7 |
Voltage unbalance |
||||||
|
– |
P/H |
– |
– |
8 |
Maximum power |
||||||
|
– |
P/H |
– |
– |
9 |
Reverse power |
||||||
|
– |
P/H |
– |
– |
10 |
Minimum frequency |
||||||
|
– |
P/H |
– |
– |
11 |
Maximum frequency |
||||||
|
– |
P/H |
– |
– |
12 |
Phase rotation |
||||||
|
– |
P/H |
– |
– |
13 |
Load shedding based on the current |
||||||
|
– |
P/H |
– |
– |
14 |
Load shedding based on the power |
||||||
|
– |
P/H |
E |
– |
15 |
If this bit is at 1, bits 0 to 14 are not valid. |
||||||
|
0x2EE9 |
12010 |
R |
– |
INT16U |
– |
– |
P/H |
– |
– |
– |
Continuation of the previous register |
|
– |
P/H |
– |
– |
0 |
Ground-fault alarm |
||||||
|
E |
P/H |
– |
– |
1 |
Earth-leakage alarm |
||||||
|
– |
– |
– |
– |
2–14 |
Reserved |
||||||
|
– |
P/H |
E |
– |
15 |
If this bit is at 1, bits 0 to 14 are not valid. |
Alarms
The alarm register provides information about the pre-alarms and the user-defined alarms. A bit is set to 1 once an alarm is active.
|
Address |
Register |
RW |
Unit |
Type |
Range |
A/E |
A/E/P/H |
Active |
X |
Bit |
Description |
|---|---|---|---|---|---|---|---|---|---|---|---|
|
0x2EEA |
12011 |
R |
– |
INT16U |
– |
A/E |
– |
– |
X |
– |
Pre-alarm register |
|
A/E |
– |
A/E |
X |
0 |
Long-time protection time pre-alarm (PAL Ir) |
||||||
|
E |
– |
– |
– |
1 |
Earth-leakage protection pre-alarm (PAL IΔn) |
||||||
|
– |
– |
– |
X |
Earth-leakage alarm(1) |
|||||||
|
A/E |
– |
– |
– |
2 |
Ground-fault protection pre-alarm (PAL Ig) |
||||||
|
– |
– |
– |
X |
Ground-fault alarm(2) |
|||||||
|
– |
– |
– |
– |
3–14 |
Reserved |
||||||
|
A/E |
– |
– |
X |
15 |
If this bit is at 1, bits 0 to 14 are not valid. |
||||||
|
0x2EEB |
12012 |
R |
– |
INT16U |
– |
A/E |
– |
– |
– |
– |
Register of user-defined alarms |
|
A/E |
– |
– |
– |
0 |
User-defined alarm 201 |
||||||
|
A/E |
– |
– |
– |
1 |
User-defined alarm 202 |
||||||
|
A/E |
– |
– |
– |
2 |
User-defined alarm 203 |
||||||
|
A/E |
– |
– |
– |
3 |
User-defined alarm 204 |
||||||
|
A/E |
– |
– |
– |
4 |
User-defined alarm 205 |
||||||
|
A/E |
– |
– |
– |
5 |
User-defined alarm 206 |
||||||
|
A/E |
– |
– |
– |
6 |
User-defined alarm 207 |
||||||
|
A/E |
– |
– |
– |
7 |
User-defined alarm 208 |
||||||
|
A/E |
– |
– |
– |
8 |
User-defined alarm 209 |
||||||
|
A/E |
– |
– |
– |
9 |
User-defined alarm 210 |
||||||
|
– |
– |
– |
– |
10–14 |
Reserved |
||||||
|
A/E |
– |
– |
– |
15 |
If this bit is at 1, bits 0 to 14 are not valid. |
||||||
|
0x2EEC– 0x2EEE |
12013– 12015 |
– |
– |
– |
– |
– |
– |
– |
– |
– |
Reserved |
|
(1) Value available on MicroLogic 7.0 X control unit only when the Digital Module ANSI 51N/51G Ground-fault alarm is installed. (2) Value available on MicroLogic 2.0 X, 3.0 X, 5.0 X, and 6.0 X control units only when the Digital Module ANSI 51N/51G Ground-fault alarm is installed. |
|||||||||||
Current
|
Address |
Register |
RW |
Unit |
Type |
Range |
A/E |
A/E/P/H |
Active |
X |
Description |
|---|---|---|---|---|---|---|---|---|---|---|
|
0x2EEF |
12016 |
R |
A |
INT16U |
0–32767 |
A/E |
A/E/P/H |
A/E |
X |
RMS current on phase 1: I1 |
|
0x2EF0 |
12017 |
R |
A |
INT16U |
0–32767 |
A/E |
A/E/P/H |
A/E |
X |
RMS current on phase 2: I2 |
|
0x2EF1 |
12018 |
R |
A |
INT16U |
0–32767 |
A/E |
A/E/P/H |
A/E |
X |
RMS current on phase 3: I3 |
|
0x2EF2 |
12019 |
R |
A |
INT16U |
0–32767 |
A/E |
A/E/P/H |
A/E |
X |
RMS current on the neutral: IN (1) |
|
0x2EF3 |
12020 |
R |
A |
INT16U |
0–32767 |
A/E |
A/E/P/H |
A/E |
X |
Maximum of I1, I2, I3, and IN |
|
0x2EF4 |
12021 |
R |
%Ig |
INT16U |
0–32767 |
A/E |
A/E/P/H |
A/E |
X |
Ground-fault current Ig (2) |
|
0x2EF5 |
12022 |
R |
%lΔn |
INT16U |
0–32767 |
E |
A/P/H |
A/P/H |
X |
Earth-leakage current IΔn (3) |
|
(1) This value cannot be accessed for motor applications and in cases of three-pole circuit breakers without external neutral current transformer (ENCT). (2) This value is only available:
(3) This value is only available:
|
||||||||||
Maximum Current Values
Maximum current values can be reset with the reset minimum/maximum command.
|
Address |
Register |
RW |
Unit |
Type |
Range |
A/E |
A/E/P/H |
Active |
X |
Description |
|---|---|---|---|---|---|---|---|---|---|---|
|
0x2EF6 |
12023 |
R |
A |
INT16U |
0–32767 |
A/E |
A/E/P/H |
A/E |
X |
Maximum RMS current on phase 1: I1 |
|
0x2EF7 |
12024 |
R |
A |
INT16U |
0–32767 |
A/E |
A/E/P/H |
A/E |
X |
Maximum RMS current on phase 2: I2 |
|
0x2EF8 |
12025 |
R |
A |
INT16U |
0–32767 |
A/E |
A/E/P/H |
A/E |
X |
Maximum RMS current on phase 3: I3 |
|
0x2EF9 |
12026 |
R |
A |
INT16U |
0–32767 |
A/E |
A/E/P/H |
A/E |
X |
Maximum RMS current on the neutral: IN (1) |
|
0x2EFA |
12027 |
R |
A |
INT16U |
0–32767 |
A/E |
A/E/P/H |
A/E |
X |
Maximum RMS current out of the 4 previous registers |
|
0x2EFB |
12028 |
R |
%Ig |
INT16U |
0–32767 |
A/E |
A/E/P/H |
A/E |
X |
Maximum ground-fault current Ig (2) |
|
0x2EFC |
12029 |
R |
%lΔn |
INT16U |
0–32767 |
E |
A/P/H |
A/P/H |
X |
Maximum earth-leakage current (3) |
|
(1) This value cannot be accessed for motor applications and in cases of three-pole circuit breakers without external neutral current transformer (ENCT). (2) This value is only available:
(3) This value is only available:
|
||||||||||
Voltage
|
Address |
Register |
RW |
Unit |
Type |
Range |
A/E |
A/E/P/H |
Active |
X |
Description |
|---|---|---|---|---|---|---|---|---|---|---|
|
0x2EFD |
12030 |
R |
V |
INT16U |
0–1200 |
E |
E/P/H |
E |
X |
RMS phase-to-phase voltage V12 |
|
0x2EFE |
12031 |
R |
V |
INT16U |
0–1200 |
E |
E/P/H |
E |
X |
RMS phase-to-phase voltage V23 |
|
0x2EFF |
12032 |
R |
V |
INT16U |
0–1200 |
E |
E/P/H |
E |
X |
RMS phase-to-phase voltage V31 |
|
0x2F00 |
12033 |
R |
V |
INT16U |
0–1200 |
E |
E/P/H |
E |
X |
RMS phase-to-neutral voltage V1N (1) |
|
0x2F01 |
12034 |
R |
V |
INT16U |
0–1200 |
E |
E/P/H |
E |
X |
RMS phase-to-neutral voltage V2N (1) |
|
0x2F02 |
12035 |
R |
V |
INT16U |
0–1200 |
E |
E/P/H |
E |
X |
RMS phase-to-neutral voltage V3N (1) |
|
(1) This value cannot be accessed for motor applications and in cases of three-pole circuit breakers without external neutral voltage transformer (ENVT). |
||||||||||
Frequency
When the MicroLogic trip unit cannot calculate the frequency, it returns Not applicable = 32768 (0x8000).
|
Address |
Register |
RW |
Unit |
Type |
Range |
A/E |
A/E/P/H |
Active |
X |
Description |
|---|---|---|---|---|---|---|---|---|---|---|
|
0x2F03 |
12036 |
R |
0.1 Hz |
INT16U |
400–600 |
E |
P/H |
E |
X |
Frequency |
|
0x2F04 |
12037 |
R |
0.1 Hz |
INT16U |
400–600 |
E |
P/H |
E |
X |
Maximum frequency (1) |
|
(1) This value can be reset with the reset minimum/maximum command. |
||||||||||
Power
|
Address |
Register |
RW |
Unit |
Type |
Range |
A/E |
A/E/P/H |
Active |
X |
Description |
|---|---|---|---|---|---|---|---|---|---|---|
|
0x2F05 |
12038 |
R |
0.1 kW |
INT16 |
-32767–+32767 |
E |
E/P/H |
E |
X |
Active power on phase 1: P1 (1) (2) |
|
0x2F06 |
12039 |
R |
0.1 kW |
INT16 |
-32767–+32767 |
E |
E/P/H |
E |
X |
Active power on phase 2: P2 (1) (2) |
|
0x2F07 |
12040 |
R |
0.1 kW |
INT16 |
-32767–+32767 |
E |
E/P/H |
E |
X |
Active power on phase 3: P3 (1) (2) |
|
0x2F08 |
12041 |
R |
0.1 kW |
INT16 |
-32767–+32767 |
E |
E/P/H |
E |
X |
Total active power: Ptot (2) |
|
0x2F09 |
12042 |
R |
0.1 kvar |
INT16 |
-32767–+32767 |
E |
E/P/H |
E |
X |
Reactive power on phase 1: Q1 (1) (2) |
|
0x2F0A |
12043 |
R |
0.1 kvar |
INT16 |
-32767–+32767 |
E |
E/P/H |
E |
X |
Reactive power on phase 2: Q2 (1) (2) |
|
0x2F0B |
12044 |
R |
0.1 kvar |
INT16 |
-32767–+32767 |
E |
E/P/H |
E |
X |
Reactive power on phase 3: Q3 (1) (2) |
|
0x2F0C |
12045 |
R |
0.1 kvar |
INT16 |
-32767–+32767 |
E |
E/P/H |
E |
X |
Total reactive power: Qtot (2) |
|
0x2F0D |
12046 |
R |
0.1 kVA |
INT16U |
0–32767 |
E |
E/P/H |
E |
X |
Apparent power on phase 1: S1 (1) |
|
0x2F0E |
12047 |
R |
0.1 kVA |
INT16U |
0–32767 |
E |
E/P/H |
E |
X |
Apparent power on phase 2: S2 (1) |
|
0x2F0F |
12048 |
R |
0.1 kVA |
INT16U |
0–32767 |
E |
E/P/H |
E |
X |
Apparent power on phase 3: S3 (1) |
|
0x2F10 |
12049 |
R |
0.1 kVA |
INT16U |
0–32767 |
E |
E/P/H |
E |
X |
Total apparent power: Stot |
|
(1) This value cannot be accessed for motor applications and in cases of three-pole circuit breakers without external neutral current transformer (ENCT). (2) The sign for the active and reactive power depends on the configuration of:
|
||||||||||
Energy
Energy is stored in big-endian format: the most significant register is transmitted first, the least significant second.
|
Address |
Register |
RW |
Unit |
Type |
Range |
A/E |
A/E/P/H |
Active |
X |
Description |
|---|---|---|---|---|---|---|---|---|---|---|
|
0x2F11–0x2F12 |
12050–12051 |
R |
kWh |
INT32 |
-1 999 999 999– |
E |
E/P/H |
E |
X |
Active energy: Ep (1) |
|
0x2F13–0x2F14 |
12052–12053 |
R |
kvarh |
INT32 |
-1 999 999 999– +1 999 999 999 |
E |
E/P/H |
E |
X |
Reactive energy: Eq (1) |
|
0x2F15–0x2F16 |
12054–12055 |
R |
kWh |
INT32U |
0–1 999 999 999 |
E |
P/H |
E |
X |
Active energy counted positively: EpIn |
|
0x2F17–0x2F18 |
12056–12057 |
R |
kWh |
INT32U |
0–1 999 999 999 |
E |
P/H |
E |
X |
Active energy counted negatively: EpOut |
|
0x2F19–0x2F1A |
12058–12059 |
R |
kvarh |
INT32U |
0–1 999 999 999 |
E |
P/H |
E |
X |
Reactive energy counted positively: EqIn |
|
0x2F1B–0x2F1C |
12060–12061 |
R |
kvarh |
INT32U |
0–1 999 999 999 |
E |
P/H |
E |
X |
Reactive energy counted negatively: EqOut |
|
0x2F1D–0x2F1E |
12062–12063 |
R |
kVAh |
INT32U |
0–1 999 999 999 |
E |
E/P/H |
E |
X |
Total apparent energy: Es |
|
0x2F1F–0x2F20 |
12064–12065 |
R |
kWh |
INT32U |
0–1 999 999 999 |
E |
– |
– |
X |
Active energy counted positively (non-resettable): EpIn |
|
0x2F21–0x2F22 |
12066–12067 |
R |
kWh |
INT32U |
0–1 999 999 999 |
E |
– |
– |
X |
Active energy counted negatively (non-resettable): EpOut |
|
0x2F23–0x2F2E |
12068–12079 |
– |
– |
– |
– |
– |
– |
– |
– |
Reserved |
|
(1) This value is always positive with MicroLogic E trip units for MasterPacT NT/NW, ComPacT NS and PowerPacT P- and R-frame circuit breakers. |
||||||||||
To view the correct energy values, It is recommended to update the firmware of BSCM Modbus SL/ULP module to the latest version.
The following table displays the example of correct and incorrect energy values for registers:
| Register | Description |
Incorrect Value with Firmware Version 001.000.000 |
Correct Value with Firmware Version ≥ 001.001.000 |
Unit |
|---|---|---|---|---|
| 12054–12055 |
Active energy counted positively: EpIn |
0 | 0 | kWh |
| 12056–12057 |
Active energy counted negatively: EpOut |
32000 | 32 | kWh |
| 12058–12059 |
Reactive energy counted positively: EqIn |
20000 | 20 | kVARh |
| 12060–12061 |
Reactive energy counted negatively: EqOut |
166000 | 166 | kVARh |
| 12062–12063 |
Total apparent energy: Es |
150000 | 150 | kVAh |
| 12064–12065 |
Active energy counted positively (non-resettable): EpIn |
0 | 0 | kWh |
| 12066–12067 |
Active energy counted negatively (non-resettable): EpOut |
159000 | 159 | kWh |
Current Demand Values
|
Address |
Register |
RW |
Unit |
Type |
Range |
A/E |
A/E/P/H |
Active |
X |
Description |
|---|---|---|---|---|---|---|---|---|---|---|
|
0x2F2F |
12080 |
R |
A |
INT16U |
0–32767 |
E |
E/P/H |
E |
X |
Current demand value on phase 1: I1 Dmd |
|
0x2F30 |
12081 |
R |
A |
INT16U |
0–32767 |
E |
E/P/H |
E |
X |
Current demand value on phase 2: I2 Dmd |
|
0x2F31 |
12082 |
R |
A |
INT16U |
0–32767 |
E |
E/P/H |
E |
X |
Current demand value on phase 3: I3 Dmd |
|
0x2F32 |
12083 |
R |
A |
INT16U |
0–32767 |
E |
E/P/H |
E |
X |
Current demand value on the neutral: IN Dmd (1) |
|
(1) This value cannot be accessed for motor applications and in cases of three-pole circuit breakers without external neutral current transformer (ENCT). |
||||||||||
Power Demand Values
-
For the block window, the demand value is updated at the end of the window.
-
For the sliding window,
-
If window duration is configured for less or equal to 15 minutes, the demand value is updated every 15 seconds
-
If window duration is configured for more than 15 minutes, the demand value is updated every 1 minute.
-
|
Address |
Register |
RW |
Unit |
Type |
Range |
A/E |
A/E/P/H |
Active |
X |
Description |
|---|---|---|---|---|---|---|---|---|---|---|
|
0x2F33 |
12084 |
R |
0.1 kW |
INT16U |
0–32767 |
E |
E/P/H |
E |
X |
Total active power demand: P Dmd |
|
0x2F34 |
12085 |
R |
0.1 kvar |
INT16U |
0–32767 |
E |
P/H |
E |
X |
Total reactive power demand: Q Dmd |
|
0x2F35 |
12086 |
R |
0.1 kVA |
INT16U |
0–32767 |
E |
P/H |
E |
X |
Total apparent power demand: S Dmd |
|
0x2F36– 0x2F38 |
12087– 12089 |
– |
– |
– |
– |
– |
– |
– |
– |
Reserved |
Maximum Voltage Values
Maximum voltage values can be reset with the reset minimum/maximum command.
Register = 0 if the voltage < 25 V.
|
Address |
Register |
RW |
Unit |
Type |
Range |
A/E |
A/E/P/H |
Active |
X |
Description |
|---|---|---|---|---|---|---|---|---|---|---|
|
0x2F39 |
12090 |
R |
V |
INT16U |
0–1200 |
E |
E/P/H |
E |
X |
Maximum RMS phase-to-phase voltage V12 |
|
0x2F3A |
12091 |
R |
V |
INT16U |
0–1200 |
E |
E/P/H |
E |
X |
Maximum RMS phase-to-phase voltage V23 |
|
0x2F3B |
12092 |
R |
V |
INT16U |
0–1200 |
E |
E/P/H |
E |
X |
Maximum RMS phase-to-phase voltage V31 |
|
0x2F3C |
12093 |
R |
V |
INT16U |
0–1200 |
E |
E/P/H |
E |
X |
Maximum RMS phase-to-neutral voltage V1N (1) |
|
0x2F3D |
12094 |
R |
V |
INT16U |
0–1200 |
E |
E/P/H |
E |
X |
Maximum RMS phase-to-neutral voltage V2N (1) |
|
0x2F3E |
12095 |
R |
V |
INT16U |
0–1200 |
E |
E/P/H |
E |
X |
Maximum RMS phase-to-neutral voltage V3N (1) |
|
(1) This value cannot be accessed for motor applications and in cases of three-pole circuit breakers without external neutral voltage transformer (ENVT). |
||||||||||
Power Factor
The sign for the fundamental power factor (cosϕ) depends on the MicroLogic configuration.
|
Address |
Register |
RW |
Unit |
Type |
Range |
A/E |
A/E/P/H |
Active |
X |
Description |
|---|---|---|---|---|---|---|---|---|---|---|
|
0x2F3F |
12096 |
R |
0.01 |
INT16 |
-100– +100 |
E |
E/P/H |
E |
X |
Power factor on phase 1: PF1 (1) |
|
0x2F40 |
12097 |
R |
0.01 |
INT16 |
-100– +100 |
E |
E/P/H |
E |
X |
Power factor on phase 2: PF2 (1) |
|
0x2F41 |
12098 |
R |
0.01 |
INT16 |
-100– +100 |
E |
E/P/H |
E |
X |
Power factor on phase 3: PF3 (1) |
|
0x2F42 |
12099 |
R |
0.01 |
INT16 |
-100– +100 |
E |
E/P/H |
E |
X |
Total power factor: PF |
|
0x2F43 |
12100 |
R |
0.01 |
INT16 |
-100– +100 |
E |
H |
– |
X |
Fundamental power factor on phase 1: cosϕ1 (1) |
|
0x2F44 |
12101 |
R |
0.01 |
INT16 |
-100– +100 |
E |
H |
– |
X |
Fundamental power factor on phase 2: cosϕ2 (1) |
|
0x2F45 |
12102 |
R |
0.01 |
INT16 |
-100– +100 |
E |
H |
– |
X |
Fundamental power factor on phase 3: cosϕ3 (1) |
|
0x2F46 |
12103 |
R |
0.01 |
INT16 |
-100– +100 |
E |
H |
– |
X |
Total fundamental power factor: cosϕ |
|
(1) This value cannot be accessed for motor applications and in cases of three-pole circuit breakers without external neutral voltage transformer (ENVT). |
||||||||||
Total Harmonic Distortion (THD)
|
Address |
Register |
RW |
Unit |
Type |
Range |
A/E |
A/E/P/H |
Active |
X |
Description |
|---|---|---|---|---|---|---|---|---|---|---|
|
0x2F47 |
12104 |
R |
0.1 % |
INT16U |
0–5000 |
E |
H |
– |
X |
Total harmonic distortion of V12 compared to the fundamental |
|
0x2F48 |
12105 |
R |
0.1 % |
INT16U |
0–5000 |
E |
H |
– |
X |
Total harmonic distortion of V23 compared to the fundamental |
|
0x2F49 |
12106 |
R |
0.1 % |
INT16U |
0–5000 |
E |
H |
– |
X |
Total harmonic distortion of V31 compared to the fundamental |
|
0x2F4A |
12107 |
R |
0.1 % |
INT16U |
0–5000 |
E |
H |
– |
X |
Total harmonic distortion of V1N compared to the fundamental (1) |
|
0x2F4B |
12108 |
R |
0.1 % |
INT16U |
0–5000 |
E |
H |
– |
X |
Total harmonic distortion of V2N compared to the fundamental (1) |
|
0x2F4C |
12109 |
R |
0.1 % |
INT16U |
0–5000 |
E |
H |
– |
X |
Total harmonic distortion of V3N compared to the fundamental (1) |
|
0x2F4D |
12110 |
R |
0.1 % |
INT16U |
0–5000 |
E |
H |
– |
X |
Total harmonic distortion of I1 compared to the fundamental |
|
0x2F4E |
12111 |
R |
0.1 % |
INT16U |
0–5000 |
E |
H |
– |
X |
Total harmonic distortion of I2 compared to the fundamental |
|
0x2F4F |
12112 |
R |
0.1 % |
INT16U |
0–5000 |
E |
H |
– |
X |
Total harmonic distortion of I3 compared to the fundamental |
|
0x2F50 |
12113 |
R |
0.1 % |
INT16U |
0–5000 |
E |
H |
– |
X |
Total harmonic distortion of total current compared to the fundamental |
|
(1) This value cannot be accessed for motor applications and in cases of three-pole circuit breakers without external neutral voltage transformer (ENVT). |
||||||||||