GEX2564100SWE-00(NORDICS)

Access to Switching Device Compartment

DANGER
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
Open the switching device compartment only if the truck is in disconnected position. Refer to Operation — Racking-out the truck from service into disconnected position in User Manual.
Failure to follow these instructions will result in death or serious injury.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?