GEX2564100SWE-00(NORDICS)

Removing the Circuit Breaker from the Panel

Coupling the Transport Trolley to the Panel

Follow the below steps to couple the transport trolley to the panel:

  1. Adjust rails and unlocking bar of trolley to the correct track width of the circuit breaker (see Transport Trolley for Circuit Breaker).

  2. Turn lever to the left (Figure 32, 1).

    The trolley is lifted on the front.

  3. Move trolley to the panel so that the lateral guides (Figure 33, 2) are close to the panel, and turn lever (1) back to the right. The trolley is locked on the panel (3).

Figure 32
Turning lever on trolley to the left

Figure 33
Locking transport trolley on panel

Remove Panel

Follow the below steps to remove the panel:

  1. Push unlocking bar (Figure 34, 4) forward to its stop.

    The latching of the circuit breaker in the panel is released.

  2. Pull the circuit breaker onto the trolley via the two handles (5) until it snaps in on the trolley audibly.

  3. Turn lever back to the left (6).

    The trolley is lifted on the front, and removed from the panel.

  4. Pull trolley with the circuit breaker away from the panel (7) and turn lever back to the right to lower it (8).

Figure 34
Pull circuit breaker onto trolley

Figure 35
Pull circuit breaker onto trolley

Now the circuit breaker can be raised by means of a crane, and deposited.

For more information, see Circuit Breakers. Instructions regarding lifting and transporting trucks (EvoPact HVX, UTX, MTX and CVX).

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?