GEX2564100SWE-00(NORDICS)

Removing and Connecting the Low Voltage Connector

NOTICE
hazard of incorrect operation
Remove or insert the low-voltage connector only if the truck is in disconnected position.
Failure to follow these instructions can result in equipment damage.

Removing the Low-Voltage Connector

Follow the below steps to remove the low voltage connector:

  1. Pull interlocking slide of low voltage connector forward (Figure 30, 1) and remove the connector (2).

  2. Stow low-voltage connector in storage tray above the circuit breaker (Figure 31).

Figure 30
Removing the low-voltage connector

Figure 31
Place low-voltage connector in tray above the circuit breaker

Connecting the Low-Voltage Connector

Follow the below steps to connect the low voltage connector:

  1. Take low-voltage connector from the storage tray above the circuit breaker (Figure 31).

  2. Insert low-voltage connector into the circuit breaker and press interlocking slide forward.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?