GEX2564100SWE-00(NORDICS)

Auxiliary Products

WARNING
hazard oF INAPPROPRIATE HANDLING
Observe the safety data sheets of the manufacturers of the auxiliary products.
Failure to follow these instructions can result in death, serious injury, or equipment damage.

Auxiliary product

Order number

Cleaning agent

S008152

Lubricant KL, 0.5 kg can

ST312-111-835

Liquid lubricant FL, 0.5 kg can

S008153

Repair paint, 500 g can, RAL 7044, silk-grey

S009 492

The auxiliary products are available from the manufacturer. The use of alternative auxiliary products is not permissible.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?