GEX2564100SWE-00(NORDICS)

Overview of Cable Connection System

Cable connection variants:

Cable connection for Ø 13: Cable cross section ≤ 400 mm2

Cable connection for 4 bore-holes of Ø 9: Cable cross section 500 or 630 mm2

Figure 57
Connecting bar 80 x 10 with dimensions for the fastening of cable sealing end

Overview of cable connection variants

Cable terminal per phase

Representation of a connection phase

Front view

Side view

max. 2

max. 4

max. 6

max. 8

Further cable connection variants optionally available:

Clarify technical details and design specifications with the manufacturer, as required.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?