GEX2564100SWE-00(NORDICS)

Dimensions and Weights (Without Packaging)

For the precise panel dimensions, refer to the switchgear-specific documentation. These depend on:

  • the rated voltage

  • the rated normal current

  • the rated short-time current and

  • additional equipment:

    • busbar or fan attachments

    • rear high voltage cable connection

Figure 14
Dimensions of PIX panels

a Panel width

b Panel height (depending on height of low-voltage compartment)

c Height of low-voltage compartment

d Panel height without low-voltage compartment and attachments

e Panel depth

Figure 15
Dimensions of pressure relief duct

1 Pressure relief duct

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?