GEX2564100SWE-00(NORDICS)

Transport of the Panels/Circuit Breakers on the Construction Site

WARNING
hazard of incorrect operation
  • Make sure the rope or the chain being used is strong enough to bear the weight of the panel (see Dimensions and Weights (Without Packaging)). Comply with the relevant provisions for hoisting equipment.
  • On lowering the panels, make sure that the supporting platform is sufficiently stable and even.
  • Pay attention to floor openings.
Failure to follow these instructions can result in death, serious injury, or equipment damage.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?