GEX2564100SWE-00(NORDICS)

Opening and Closing the Front Door

Opening the Front Door

Follow the below steps to open the front door:

  1. Insert double-bit key into the door opening and turn it to the left (Figure 27, 1).

    The door is unlocked.

  2. Insert handle with the lever pointing down, and turn handle to the left (2).

    The front door is lifted.

  3. To open the door, swing it to the left (3).

Figure 27
Opening the front door

Closing the Front Door

Follow the below steps to close the front door:

  1. Close the door completely.

  2. Turn the handle downwards; the door is lowered.

  3. Pull door handle off and stow it in the tool tray of the trolley (see Operation Accessories).

  4. Lock the door using a double-bit key

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?