GEX2564100SWE-00(NORDICS)

Access to the Busbar Compartment

DANGER
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
Open the busbar compartment only if the busbar is earthed. Refer to Operation — Earthing the busbar in User Manual.
Failure to follow these instructions will result in death or serious injury.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?