Connection of High-Voltage Cables
Preparation of Cable Compartment
Access to cable compartment: see Access to the Cable Compartment.
-
Release fastening of cable clips (Figure 59, 1).
-
Remove cable clips (2).
-
Remove rubber sleeves (3).
-
Remove base plate (4) as required.
Mount Sealing End and Cable Lug
CAUTION |
|---|
|
HAZARD OF INAPPROPRIATE ASSEMBLY
Failure to follow these instructions can result in injury or equipment damage.
|
Follow the below steps to mount sealing end:
-
Route the individual cables outwards through the cable compartment of the panel to enable assembly of the cable ends.
-
Cut the rubber sleeves to fit the cable diameter, and push them onto the cables (Figure 60).
-
Strip cable ends and assemble the sealing end as specified by the cable manufacturer.
Follow the below steps to mount cable lug:
-
Fasten the individual cables to the appropriate connection surfaces (Figure 62 to Figure 64). In case of two cables per phase: Connect the two cables to the first connection (Figure 63).
-
Re-mount the base plates.
-
Fasten high-voltage cable to the base plates using clamping assemblies (Figure 65 and Figure 66).
-
Screw-fasten the earthing screens (2) of the cables to the earthing bar (3) of the panel.
|
1 High-voltage cable |
2 Earthing screen |
3 Earthing bar |
|
Figure 63 |
Figure
64 |
|
Figure 65 |
Figure 66 |
CAUTION