GEX2564100SWE-00(NORDICS)

Access to the Cable Compartment

DANGER
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
Open the cable compartment only if the earthing switch is ON. Refer to Operation — Switching ON the Earthing Switch in User Manual.
Failure to follow these instructions will result in death or serious injury.

The panels can be equipped with supplementary cylinder locks to lock the cable compartment cover. Refer to Operation — Interlocks in User Manual.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?