Low-Voltage Connection
Normally the low-voltage compartment is already mounted on top of the panel when delivered to site. In some cases both components - high-voltage part and low-voltage part can be delivered separately.
Follow the below steps to connect the low-voltage compartment.
-
Remove transport protection covers. Assign the low-voltage compartment to the appropriate panel.
-
Position low-voltage compartment carefully on top of the panel, verifying that the top internal connection cables of the panel are not damaged.
-
Align low-voltage compartment and screw-fasten it to the panel. Assembly drawing: AGS C73 180-01 .
-
Screw-fasten the low-voltage compartments to each other at the sides.
-
Connect the panel’s internal terminals for control and measuring cables according to the connector identification and the circuit diagram to the terminal strips in the low-voltage compartment.
Access to the Low-Voltage Compartment
Follow the below steps to access to the low-voltage compartment.
-
Insert double-bit key into the lock of the low-voltage compartment and turn it to the left by 90°.
-
Open door to the left.
-
The door can be secured optionally in open position using a lock plate (Figure 68, 1).
|
1 |
Lock plate (optional) |
|
2 |
Ring circuits |